搭配功率产品,运行一两天会偶发性出现一次复位现象,监控XRS引脚为低电平复位,持续时间每次都是51.2us,有使用电源监测芯片监测1.2V、3.3V、5V,非电源监测芯片输出的复位信号,想请教各位大神,这种情况是什么导致的,有哪些情况会出现这样的复位现象?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
搭配功率产品,运行一两天会偶发性出现一次复位现象,监控XRS引脚为低电平复位,持续时间每次都是51.2us,有使用电源监测芯片监测1.2V、3.3V、5V,非电源监测芯片输出的复位信号,想请教各位大神,这种情况是什么导致的,有哪些情况会出现这样的复位现象?
您好
TMS320F28379D偶发性复位问题分析
复位现象描述:TMS320F28379D在运行一两天后偶发性复位,XRS引脚为低电平,持续时间51.2us,非电源监测芯片输出复位信号。
可能原因:
建议:检查并初始化所有变量,确保无溢出;优化串口通信错误处理;谨慎管理内存使用,避免大数组导致的问题
您好
针对您描述的TMS320F28379D搭配功率产品出现的偶发性复位现象,这里列出一些可能的原因和排查建议。由于复位是由XRS引脚低电平触发,且持续时间固定为51.2us,这通常指向外部事件或特定的系统状态异常。以下是一些可能的原因:
外部干扰:
硬件问题:
软件与配置:
环境与外部因素:
调试与测试:
您好
在TMS320F28379D(或任何类似的DSP处理器)中,是否会导致DSP复位取决于多个因素,包括函数的性质、资源的使用(如寄存器、内存)、中断的优先级和处理机制,以及任务的同步和互斥处理。
资源竞争和冲突:
中断优先级和任务调度:
堆栈溢出:
硬件异常: