This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: VDDIO至main函数耗时太长

Part Number: TMS320F280039C


在开发板上测试发现,VDDIO上电至main函数耗时130ms左右,耗时太长了,我们的项目需要控制在20ms以内。第一问我需要怎么做;第二问是什么造成耗时130ms的

测试方式:main函数第一句进行GPIO6初始化,并拉高。

以下为main函数代码:

void main(void){
GpioCtrlRegs.GPAODR.bit.GPIO6     = 0;        
GpioCtrlRegs.GPAPUD.bit.GPIO6     = 0; 
GpioCtrlRegs.GPAINV.bit.GPIO6     = 0;   
GpioCtrlRegs.GPAQSEL1.bit.GPIO6   = 0;  
GpioCtrlRegs.GPADIR.bit.GPIO6     = 1;
GpioCtrlRegs.GPACSEL1.bit.GPIO6   = 0;  
GpioCtrlRegs.GPAMUX1.bit.GPIO6    = 0;   
GpioDataRegs.GPACLEAR.bit.GPIO6   = 1;

GpioDataRegs.GPASET.bit.GPIO6 = 1;
.............
}