This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我设置的ADC开始转换为EPWM触发转换,那么ADC的采样频率是不是就是EPWM的频率(触发ADC转换条件为CTR=0),如果是,那么如果我的EPWM的频率不是很高,假如4K,那么ADC的转换也只有4K,会不会导致波形失真。
一般应用,adc频率=epwm频率=控制频率
其实这主要看你的控制系统的设计,控制频率直接关系到你的整个系统。一般而言adc频率>=控制频率,而控制频率=epwm频率,但是也不尽然,还得具体分析。
具体项目中,首先考虑控制频率。
如果只是两路,三路采样 4K对于C2000 ADC应该没有问题。ADC的采样精度应该可以保证,你可以把采样窗开到10个cycle以上,都完全来的及。