如题,由于CCS5中bios5x的调试分析功能不完整,并且升级到bios6过程较长,我们希望继续使用ccs3.3 & bios5x
请教可行的解决方案 & 仿真器xd100能在3,3上运作指南?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以用CCS3.3对工程进行编译,用CCS4或者CCS5进行下载。
我就是这样用的,CCS3.3和CCS5对于F28069来说,编译都是靠CGT来做的,与CCS版本无关。
唯一的区别就是CCS3.3的烧写插件不支持F28069,而CCSv5的支持。
所以楼主可以用CCS3.3进行编译,连接的时候选择F28035就可以,CMD文件改成F28069的即可。
仿真器都选XDS100就可以了,无论在CCS3.3或者CCSv5上。
可以在CCS3.3下进行仿真,但要导入.out文件的镜像,File --> Load Symbol only