This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC-AC开发套件输出不是正弦波

Other Parts Discussed in Thread: CONTROLSUITE

各位专家,你们好!

我买了High Voltage Single Phase Inverter Development Kit ,型号:TMDSHV1PHINVKIT。在off-grid下,接500欧电阻负载,不管我用GUI软件还是不用,输出是方波,且用万用表AC档测量时电压361V,请专家指导解答!我拿到DEMO板时没刷程序,里面应该是有程序的,control-card上LED2每一秒闪烁一次。

  • 请参考C:\TI\controlSUITE\development_kits\HV_SOLAR_DC_AC_v1.0\~Docs第二个文档Quick Start Guide for Solar HV DC-AC Board_Rev1.2.pdf第7页2.1 The equipments表格中对Resistor Load的要求。

    建议再检查确保其它设备也都符合要求。

  • 电阻负载选80欧、90欧、100欧时会出错,GUI软件显示是DC BUS VOLTAGE UNDER ,我的DC电源是380V/2A的,用400V/2A的也不行。接250欧负载时输出也是方波。注:我没有DC-DC模块,只有DC-AC模块。

  • 请将输出负载电阻减小为25欧姆,此时输出电压应为120V左右。当离线开机时,由于程序中设置为输出恒定电流2.8A,所以,当你接入80欧以上时,输出负载在600W以上,若DC电源的动态响应不够快,可能瞬间达到DC电源的限制。所以,请将电阻减小到25欧姆,先输出120V

  • Vieri Xue,您所说的”离线开机“是什么意思?另外,文档里只说是恒流输出,没说多大,程序里在哪个文件的哪一行有这一限制?谢谢您!

  • off-grid下我接了40欧的电阻负载,用GUI选择120或220输出均为120V左右,实际测试确实为恒流输出,我测的是2.7A。上电默认为120V输出,如果要220V并网需要用GUI选择120,再选择220并使能并网选项打勾。