This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D将程序分别下载到cpu1和CPU2的flash后,断电后CPU2里的EPWM7程序未运行,该怎么办?



28377D将程序分别下载到cpu1和CPU2的flash后,断电后CPU2里的EPWM7程序未运行,该怎么办?

请各位专家老师帮忙提示一下,这个问题困扰我好多天了,谢谢

CPU1程序如下:

void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
    InitSysCtrl();
    InitIpc();
#define _STANDALONE 1
#define _FLASH  1
#ifdef _STANDALONE
#ifdef _FLASH
    //  Send boot command to allow the CPU02 application to begin execution
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else
    //  Send boot command to allow the CPU02 application to begin execution
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
    InitGpio();
    EALLOW;
     GpioCtrlRegs.GPEPUD.bit.GPIO157 = 1;    // Disable pull-up on GPIO157 (EPWM7A)
     GpioCtrlRegs.GPEPUD.bit.GPIO158 = 1;    // Disable pull-up on GPIO158 (EPWM7B)
     GpioCtrlRegs.GPEMUX2.bit.GPIO157 = 1;   // Configure GPIO157 as EPWM7A
     GpioCtrlRegs.GPEMUX2.bit.GPIO158 = 1;   // Configure GPIO158 as EPWM7B
        EDIS;
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
    DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
    InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;
    IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
    InitPieVectTable();
    MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
    InitFlash();
// Enable global Interrupts and higher priority real-time debug events:
    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM
// For this case just init GPIO pins for ePWM1
// Only CPU1 can configure GPIO muxing so this is done here
// These functions are in the F2837xD_EPwm.c file

    //Transfer ownership of EPWM1 and ADCA to CPU02
 EALLOW;
    DevCfgRegs.CPUSEL0.bit.EPWM7 = 1;
    EDIS;
// Step 6. IDLE loop. Just sit and loop forever (optional):
    while(1)
    {
     asm(" nop");
    }
}
MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr)
{
    while(SourceAddr < SourceEndAddr)
    {
       *DestAddr++ = *SourceAddr++;
    }
    return;
}
CPU2的程序如下:
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
    InitSysCtrl();
    InitIpc();
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//    InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
    DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
    InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
    IER = 0x0000;
    IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
    InitPieVectTable();
    MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
    InitFlash();
// Register the EPWM interrupt handler for EPWM1
    EALLOW;
 PieVectTable.EPWM7_INT = &epwm7_isr;
 EDIS;
//Power up the PWM and ADC
 EALLOW;
 CpuSysRegs.PCLKCR2.bit.EPWM7=1;
//Configure the ADC and power it up

//Setup the ADC for continuous conversions on channel 0
// Configure EPWM1
 EALLOW;
 CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
 EDIS;
 InitEPwm7Example();
 EALLOW;
 CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
 EDIS;
// Enable CPU INT3 which is connected to EPWM1 INT:
 IER |= M_INT3;
// Enable EPWM INTn in the PIE: Group 3 interrupt 1
 PieCtrlRegs.PIEIER3.bit.INTx7 = 1;
//Enable global Interrupts and higher priority real-time debug events:
    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM
//Initialize results buffer
   for(;;)
   {
   }
}
__interrupt void epwm7_isr(void)
{
    // Clear INT flag for this timer
    EPwm7Regs.ETCLR.bit.INT = 1;
    // Acknowledge this interrupt to receive more interrupts from group 3
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
void InitEPwm7Example()
{
   // Setup TBCLK
 EPwm7Regs.TBPRD = 6000;                       // Set timer period
      EPwm7Regs.TBPHS.bit.TBPHS = 0x0000;           // Phase is 0
      EPwm7Regs.TBCTR = 0x0000;                     // Clear counter
      // Setup TBCLK
      EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
      EPwm7Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable phase loading
      EPwm7Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2;       // Clock ratio to SYSCLKOUT
      EPwm7Regs.TBCTL.bit.CLKDIV = TB_DIV1;
      EPwm7Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;   // Load registers every ZERO
      EPwm7Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
      EPwm7Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
      EPwm7Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
      // Setup compare
      EPwm7Regs.CMPA.bit.CMPA = 3000;
      // Set actions
      EPwm7Regs.AQCTLA.bit.CAU = AQ_SET;            // Set PWM1A on Zero
      EPwm7Regs.AQCTLA.bit.CAD = AQ_CLEAR;
      EPwm7Regs.AQCTLB.bit.CAU = AQ_NO_ACTION;         // Set PWM1A on Zero
      EPwm7Regs.AQCTLB.bit.CAD = AQ_NO_ACTION;
      // Active Low PWMs - Setup Deadband
      EPwm7Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
      EPwm7Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
      EPwm7Regs.DBCTL.bit.IN_MODE = DBA_ALL;
      EPwm7Regs.DBRED = 1000;
      EPwm7Regs.DBFED = 1000;
      // Interrupt where we will change the Deadband
      EPwm7Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;    // Select INT on Zero event
      EPwm7Regs.ETSEL.bit.INTEN = 1;               // Enable INT
      EPwm7Regs.ETPS.bit.INTPRD = ET_1ST;          // Generate INT on 3rd event
}
MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr)
{
    while(SourceAddr < SourceEndAddr)
    {
       *DestAddr++ = *SourceAddr++;
    }
    return;
}