This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 SCI中断接收数据,每隔10ms连续发送字符串数据,30s后进入不了串口中断服务函数,请问大家有什么解决方案



用串口工具连续给28335的SCIB发送数据,以中断方式接收数据,数据前30秒左右正常进入中断服务函数,30s左右过后,无法进入中断服务函数,当时同时定时器0正常工作LED灯的闪烁无问题。SCIB配置为无FIFO中断接收发送模式。

下面为配置代码。

void scib_fifo_init(void)
{

ScibRegs.SCICCR.all =0x0007;
ScibRegs.SCICTL1.all =0x0003;
ScibRegs.SCICTL2.bit.RXBKINTENA = 1;
ScibRegs.SCICTL2.bit.TXINTENA = 1;
ScibRegs.SCIHBAUD = 0;
ScibRegs.SCILBAUD = 39;
SciaRegs.SCICCR.bit.LOOPBKENA =0;
ScibRegs.SCICTL1.bit.TXENA = 1; // SCI transmitter enable
ScibRegs.SCICTL1.bit.RXENA = 1; // SCI receiver enable
ScibRegs.SCICTL1.bit.SWRESET = 1;
}

__interrupt void scibRxIsr(void)
{

DINT;

Uint8 rcvdat;

rcvdat = ScibRegs.SCIRXBUF.all;
ScibRegs.SCITXBUF = rcvdat;

PieCtrlRegs.PIEACK.all|= PIEACK_GROUP9; // Issue PIE ACK
EINT;
}