This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280039C: XDS110 cannot be detected by PC

Part Number: LAUNCHXL-F280039C


I bought two LAUNCHXL-F280039C boards. One of them works properly with the DigitalPowerSDK examples in CCS when connected to the computer using a USB-C cable. The LED2 and LED3 on the launchpad light up blue as expected. However, the other board cannot be connected to the computer. The blue lights of LED2 and LED3 on the launchpad do not light up, and the XDS110 is not detected in the computer’s device manager under ports. What could be the cause of this issue?
我买了两个 LAUNCHXL-F280039C 板。当使用 USB-C 电缆连接到计算机时,其中一个与 CCS 中的 DigitalPowerSDK 示例一起正常工作。启动板上的 LED2 和 LED3 按预期呈蓝色亮起。但是,另一个板无法连接到计算机。Launchpad 上的 LED2 和 LED3 的蓝灯未亮起,并且未在计算机设备管理器的端口下检测到 XDS110。此问题的原因可能是什么?

You can click this link to view the description image: s2.loli.net/.../PXrADjTRL9nO4K6.jpg
您可以单击此链接查看描述图像