void scic_echoback_init()
{
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
ScicRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScicRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScicRegs.SCICTL2.all =0x0003;
ScicRegs.SCICTL2.bit.TXINTENA = 1;
ScicRegs.SCICTL2.bit.RXBKINTENA =1;
#if (CPU_FRQ_150MHZ)
ScicRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 37.5MHz.
ScicRegs.SCILBAUD =0x00E7;
#endif
#if (CPU_FRQ_100MHZ)
ScicRegs.SCIHBAUD =0x0001; // 9600 baud @LSPCLK = 20MHz.
ScicRegs.SCILBAUD =0x0044;
#endif
ScicRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}
void scic_fifo_init()
{
ScicRegs.SCIFFTX.all=0x8000;
}
void ReceiveData()
{
while(ScicRegs.SCIRXST.bit.RXRDY ==1) // wait for XRDY =1 for empty state
{
ReceivedChar = ScicRegs.SCIRXBUF.all;
}