This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35的flash能否选择一个区域当做eeprom使用?



如果能的话参考资料在哪个文档上? 谢谢

  • 楼主你好,Concerto里面的Flash可以当作EEPROM使用的。只是使用时需要考虑好是用M3部分的Flash还是用C2000部分的

     

    目前还没有针对这个器件的示例,但楼主可以使用flash API来简化程序设计过程。附件flash_api_f28m35x.rar中包含了API的代码。

     

    同时,针对其它C2000器件,TI也有提供EEPROM模拟的应用文档,楼主可以在下面的链接中找到:

    【EEPROM Emulation With the TMS320F28xxx DSCs】

    http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=sprab69&fileType=pdf

     

     

     

    flash_api_f28m35x.rar