This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

程序固化到flash中,可以单步调试么



用Ccs3.3调试C2000系列的Dsp,将程序固化到Flash中后,可以设置断点、单步调试么?如果可以,ram仿真调试又有什么意义呢,如果是因为ram速度快,那么固化到Flash后不是也可以通过引导将程序运行到ram么?求解答,谢谢

  • Flash中单步调试, 当然是可以的.

    既然可以 RAM 运行, 为什么不支持 RAM 调试呢?

  • liangliang luan 说:

    用Ccs3.3调试C2000系列的Dsp,将程序固化到Flash中后,可以设置断点、单步调试么?如果可以,ram仿真调试又有什么意义呢,如果是因为ram速度快,那么固化到Flash后不是也可以通过引导将程序运行到ram么?求解答,谢谢

    支持flash仿真。可能是历史遗留问题。早期的时候工具没有统一(CCS3.3中就是),使用ram仿真更方便,也快速。还有就是flash毕竟还是有寿命的问题。