This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: 正常运行时操作闲置的FLASH扇区是否可行?

Part Number: TMS320F280039C

问题说明:软件正常运行时,不屏蔽中断(50kHz)的情况下,想要对闲置的FLASH扇区进行操作是否可行(PS:已知要在RAM里对FLASH进行操作,但是操作过程中会被中断打断)?

  • 您好

    关于您的这个问题,理论上可行,实际操作十分严苛,不建议这种方式操作。

    以下建议您可以参考:

    1、在中断间隔中做相关符合您需求的处理。(时间紧,且不利于优化,擦除过程可能出现问题)

    2、中断优先级调整优化。(时间相对宽松,但是可能导致中断的处理不及时,进而导致系统的效率不高等问题)