TI团队好:
我在开发f28p65x_cpu1_cia402_solution例程,现往协议栈加了一些对象字典,加完后发现程序在debug全速运行时正常,但断电后从flash加载程序偶尔会出现程序卡死的情况,请问这应当如何排查问题呢。heap size设置为0x1000,stack size设置为00x2000.以下是CMD文件的配置。
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002 /* Update the codestart location as needed */
BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001B1, length = 0x00024F
RAMM1 : origin = 0x000400, length = 0x000400
RAMD0 : origin = 0x00C000, length = 0x002000
RAMD1 : origin = 0x00E000, length = 0x002000
RAMD2 : origin = 0x01A000, length = 0x002000 /* Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0x8000. User should comment/uncomment based on core selection */
RAMD3 : origin = 0x01C000, length = 0x002000 /* Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xA000. User should comment/uncomment based on core selection */
RAMD4 : origin = 0x01E000, length = 0x002000 /* Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xC000. User should comment/uncomment based on core selection */
RAMD5 : origin = 0x020000, length = 0x002000 /* Can be mapped to either CPU1 or CPU2. When configured to CPU2, use the address 0xE000. User should comment/uncomment based on core selection */
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
/* Combining RAM LS3 and LS4 to fit .sysmem in it */
RAMLS3 : origin = 0x009800, length = 0x001000
/* RAMLS4 : origin = 0x00A000, length = 0x000800 */
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMLS8 : origin = 0x022000, length = 0x002000 /* When configured as CLA program use the address 0x4000 */
RAMLS9 : origin = 0x024000, length = 0x002000 /* When configured as CLA program use the address 0x6000 */
/* RAMLS8_CLA : origin = 0x004000, length = 0x002000 Use only if configured as CLA program memory */
/* RAMLS9_CLA : origin = 0x006000, length = 0x002000 Use only if configured as CLA program memory */
RAMGS0 : origin = 0x010000, length = 0x002000
RAMGS1 : origin = 0x012000, length = 0x002000
RAMGS2 : origin = 0x014000, length = 0x002000
RAMGS3 : origin = 0x016000, length = 0x002000
RAMGS4 : origin = 0x018000, length = 0x002000
/* Flash Banks (128 sectors each) */
FLASH_BANK0 : origin = 0x080002, length = 0x1FFFE /* Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection */
FLASH_BANK1 : origin = 0x0A0000, length = 0x20000 /* Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection */
FLASH_BANK2 : origin = 0x0C0000, length = 0x20000 /* Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection */
/* FLASH_BANK3 : origin = 0x0E0000, length = 0x20000 Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection */
/* FLASH_BANK4 : origin = 0x100000, length = 0x20000 Can be mapped to either CPU1 or CPU2. User should comment/uncomment based on core selection */
CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800
CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800
CLATOCPURAM : origin = 0x001480, length = 0x000080
CPUTOCLARAM : origin = 0x001500, length = 0x000080
CLATODMARAM : origin = 0x001680, length = 0x000080
DMATOCLARAM : origin = 0x001700, length = 0x000080
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN
.text : >> FLASH_BANK0 | FLASH_BANK1, ALIGN(8)
.cinit : > FLASH_BANK0, ALIGN(8)
.switch : > FLASH_BANK0, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMD0
#if defined(__TI_EABI__)
.bss : > RAMLS5
.bss:output : > RAMLS2
.init_array : > FLASH_BANK0, ALIGN(8)
.const : > FLASH_BANK0, ALIGN(8)
.data : > RAMGS0
.sysmem : > RAMGS1
#else
.pinit : > FLASH_BANK0, ALIGN(8)
.ebss : >> RAMLS5 | RAMLS6
.econst : > FLASH_BANK0, ALIGN(8)
.esysmem : > RAMLS5
#endif
ramgs0 : > RAMGS0, type=NOINIT
ramgs1 : > RAMGS1, type=NOINIT
#if defined(__TI_EABI__)
.TI.ramfunc : {} LOAD = FLASH_BANK0,
RUN = RAMLS0,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
#else
.TI.ramfunc : {} LOAD = FLASH_BANK0,
RUN = RAMLS0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
ALIGN(8)
#endif
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/