This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问有TMS320F28034使用can烧录程序的软件和工具吗?可以提供一下吗,谢谢!
您好,不是新问题。
文档里描述: When run as part of the boot ROM startup process, the CAN bootloader uses the on-chip oscillator with its default room temperature trim. This is sufficient for temperature-controlled manufacturing processes, but run-time firmware updates may need to work beyond 25°C.
用这种烧录方式需要25度以上。而我们现场温度可能很低,是不是无法烧录。
您好
https://www.ti.com/lit/ug/sprui10a/sprui10a.pdf?ts=1740985517713
原来的链接已经优化到以上链接上了,您如果再打不开,请您更换浏览器和网络环境。
你好,在spraby7文档里面,第一页中资料和代码下载地址:www.ti.com/.../spraby7.
这里面的资料有说明。
您好
https://dev.ti.com/tirex/explore/node?node=A__AOxaiRPXc5pi98AR6o2XUw__C2000WARE__1kRFgrO__LATEST
这是官方提供的例程和资料,您参考一下,但是没有针对性的代码。
这个spraby7的方法,是烧写到OTP的,程序涉及通讯协议,编写错了这芯片就不能用了。
另外,Uniflash烧录工具也没有OTP的烧录选项。如何烧录。
谢谢。
您好
https://software-dl.ti.com/ccs/esd/uniflash/docs/v9_0/uniflash_quick_start_guide.html
这是官方给出的指导书,请您参考Uniflash操作说明。