Part Number: TMS320F280025C
Other Parts Discussed in Thread: SYSBIOS
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.family.c28.Hwi');
BIOS.cpuFreq.lo = 100000000;
/*
* Uncomment this line to globally disable Asserts.
* All modules inherit the default from the 'Defaults' module. You
* can override these defaults on a per-module basis using Module.common$.
* Disabling Asserts will save code space and improve runtime performance.
Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;
*/
/*
* Uncomment this line to keep module names from being loaded on the target.
* The module name strings are placed in the .const section. Setting this
* parameter to false will save space in the .const section. Error and
* Assert messages will contain an "unknown module" prefix instead
* of the actual module name.
Defaults.common$.namedModule = false;
*/
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 4;
/*
* Uncomment this line to disable the Error print function.
* We lose error information when this is disabled since the errors are
* not printed. Disabling the raiseHook will save some code space if
* your app is not using System_printf() since the Error_print() function
* calls System_printf().
Error.raiseHook = null;
*/
/*
* Uncomment this line to keep Error, Assert, and Log strings from being
* loaded on the target. These strings are placed in the .const section.
* Setting this parameter to false will save space in the .const section.
* Error, Assert and Log message will print raw ids and args instead of
* a formatted message.
Text.isLoaded = false;
*/
/*
* Uncomment this line to disable the output of characters by SysMin
* when the program exits. SysMin writes characters to a circular buffer.
* This buffer can be viewed using the SysMin Output view in ROV.
SysMin.flushAtExit = false;
*/
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x800;
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x100;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 32;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
这是我的cfg文件 配置以后虽然可以正常使用多线程 但是无法使用System_printf