Part Number: TMS320F28377D
如图所示,GSRAM加起来也只有128K字节不够我的数组的存储,可以用不同的RAM进行组合吗?还有,这里面的单位KB是指的是千字还是千字节呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
如图所示,GSRAM加起来也只有128K字节不够我的数组的存储,可以用不同的RAM进行组合吗?还有,这里面的单位KB是指的是千字还是千字节呢?
2837xD_FLASH_lnk_cpu1.cmd里面GSRAM一共16块,每一块长度是0x1000也就是4096,所以GSRAM一共只有4096*16=65536个16bit数据吗?与图片不符合呀
64KW意思是指64K个16bit数据吗?这个单位不太懂。RAM若是不够,是可以组合M0、M1、DxRAM和GSRAM是吗?感谢。
您好
64KW意思是指64K个16bit数据吗?这个单位不太懂。
64KW的具体含义
RAM若是不够,是可以组合M0、M1、DxRAM和GSRAM是吗?
理论上可以,但是先建议优化数据。