This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助TI技术支持,仿真器报错“Error -1155 @ 0x0”



问题是这样的,刚开始烧写都是好的,不知道怎么回事再次下载就出错了,完整错误信息如下:

Error connecting to the target:
(Error -1155 @ 0x0)
Device may be operating in low-power mode. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.73.0)

我做了以下步骤尝试解决问题,但都失败了:

1,重新启动计算机,断电F28035开发板与XDS100V2仿真器,

2,拿已经通过的工程烧写

3,用同一个仿真器,同一个工程文件烧写另一块F28035开发板,成功,仿真器没问题

4,我把有问题的开发板再次接到仿真器,做CONNECT连接测试,也是好的,没有错误,但是烧写的时候(Error -1155 @ 0x0)错误依旧

到这里求助TI的技术支持们,现在在做项目,很着急,找不到原因,在此感谢各位了。