Part Number: TMS320F28054F
Other Parts Discussed in Thread: MOTORWARE
软件基于motorware的1_01_00_18 版本的DRV8312-KIT_revD开发
1.我在调试电机带载运行时,电流达不到项目需求,在各项参数中修改了ADC采样的转换系数 pUserParams->current_sf 该变量后(*0.7~0.8的缩放),从原先的70A左右电流提高到了90A以上。首先这个参数被修改是否合理?其次,如果不应该修改的话,其他影响最大电流的可能要调整的参数是什么?已经将USER_MAX_VS_MAG_PU修改为最大的0.6666
2.第二个问题是,在空载通过一个数字信号控制加速的过程中,如果加的过快或者给的电流环参考电流过大,电机会发生控制失步,如果解决或者限制最大电频率呢?