专家您好!
现在在使用TMS320F280049C的SCI模块FIFO功能时,如何实现一个完整数据包的接收?
比如:我的自定义数据包共有24个字节,而寄存器RXFFIL设置为16,当产生接收FIFO中断时,一次就接收16个字节,剩下的8个字节似乎没有收到,我的SCI初始化配置如下:
可以正常工作,但是我如果在串口程序一次发送24个字节,就只能正确收到16个字节。其余的8字节该用什么方式接收呢?我尽量想使用FIFO,这样可以大幅减少CPU中断次数。
//
// SCI_FIFO_Init - Configure SCIB FIFO
//
void SCI_FIFO_Init(void)
{
Uint16 i;
GPIO_SetupPinMux(13, GPIO_MUX_CPU1, 6);
GPIO_SetupPinOptions(13, GPIO_INPUT, GPIO_PUSHPULL);
GPIO_SetupPinMux(40, GPIO_MUX_CPU1, 9);
GPIO_SetupPinOptions(40, GPIO_OUTPUT, GPIO_ASYNC);
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SCIB_RX_INT = &SCI_FIFO_Rx_Isr;
PieVectTable.SCIB_TX_INT = &SCI_FIFO_Tx_Isr;
EDIS; // This is needed to disable write to EALLOW protected registers
ScibRegs.SCICCR.all = 0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScibRegs.SCICTL1.all = 0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScibRegs.SCICTL2.all = 0x0003;
ScibRegs.SCICTL2.bit.TXINTENA = 1;
ScibRegs.SCICTL2.bit.RXBKINTENA = 1;
//ScibRegs.SCIHBAUD.all = 0x0001;
//ScibRegs.SCILBAUD.all = 0x0044;
ScibRegs.SCIHBAUD.all = ((uint16_t)SCI_PRD & 0xFF00U) >> 8U;
ScibRegs.SCILBAUD.all = (uint16_t)SCI_PRD & 0x00FFU;
ScibRegs.SCICCR.bit.LOOPBKENA = 0; // Disable loop back
ScibRegs.SCIFFTX.all = 0xC030;//1100 0000 0010 0100
ScibRegs.SCIFFRX.all = 0x0030;//1100 0000 0010 0100
ScibRegs.SCIFFCT.all = 0x00;
ScibRegs.SCICTL1.all = 0x0023; // Relinquish SCI from Reset
ScibRegs.SCIFFTX.bit.TXFIFORESET = 1;
ScibRegs.SCIFFRX.bit.RXFIFORESET = 1;
for(i = 0; i<20; i++)
{
RX_BUFFER[i] = i;
}
//rdata_pointA = sdataA[0];
//
// Enable interrupts required for this example
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx3 = 1; // PIE Group 9, INT3 for RX
//PieCtrlRegs.PIEIER9.bit.INTx4 = 1; // PIE Group 9, INT4 for TX
//PieCtrlRegs.PIEIER9.bit.INTx1 = 1; // PIE Group 9, INT1
//PieCtrlRegs.PIEIER9.bit.INTx2 = 1; // PIE Group 9, INT2
IER |= 0x100; // Enable CPU INT
EINT;
ERTM;
}