This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Team:
Where can I find the software project of the TIDM-02009 design?I have search the "C2000Ware_DigitalPower_SDK_5_04_00_00" and "C2000Ware_MotorControl_SDK_5_03_00_00",there are no any information about the TIDM-02009 design.I have already made sure these two library packages are both latest version.And I also check the TIDM-02009 web page("TIDM-02009 参考设计 | 德州仪器 TI.com.cn"),there are no any software design files in design files list.
I will appreciate it that if you give me software resource of TIDM-02009 soon,Thank you very much.
Hi,
Please refer to this thread,e2e.ti.com/.../tidm-02009-tidm-02009