This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好我想问一下,我在syscfg中配置C1的SOC触发为PWM4B,但是我又在一个2MS的函数中调用了对应的强制转换SOC的寄存器,我想问一下最后的采样结果是按照syscfg配置的结果还是执行2MS函数中结果,又或者是2种都执行,目前发现会导致我的电压环响应变慢。
您好,
对延迟响应深表歉意。 我看到您已将 EPWM 配置为触发源、并且还使用了2ms 函数中的软件强制触发。 软件强制位被覆盖以启动 ADC 转换。 如果 EPWM 正在运行并在 CPU 执行此2ms 函数时触发 ADC、这两个事件(EPWM 触发和 SW 强制触发)都可以触发 ADC 以启动转换。