This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用的DSP为TMS320F280025,引脚GPIO26 GPIO27两个引脚都接了一个10K的上拉电阻,除IIC引脚外,没有对程序做任何改动。
测试pmbus_over_i2c_target_example例程,通信速率100K时,主机发送读数据请求之后,从机有给回应信号,之后SCL和SDA都被拉低,需要复位从机之后才能恢复;
通信速率400K可以正常通信。
后使用PMBUS over I2C Communications Stack源程序自建工程,测试结果一样,在调试过程中发现主机发送读请求时,在
if(TARGET_TRANSMITTER)中打断点,程序不会停止,或者nBytes = 0;
用两块板,一块作为主机运行pmbus_over_i2c_controller_example,一块作为从机运行pmbus_over_i2c_target_example在通信速率100KHz时也会出现。
请问是否有伙伴遇到过同样的情况?如何解决的?或者有无一些好的建议,求解答,谢谢!