TI的专家您好!
最近在学习TIDA-010062中LLC的源程序,看到函数LLC_updateDeadband在根据次级输出电流的不同范围值来设置ePWM的死区时间时,FED和RED在每个电流值范围都是一样的,请问是什么原因?这是要让用户根据情况自己设置吗?
截图如下,麻烦解答下,谢谢了!
This need be coordinated with the hardware.
At the beginning, when I am using Si MOSFET on the LLC primary, it is 50@range0, 45@range1, 40@range2, 35@range3, 30@range4, 25@range5.