Other Parts Discussed in Thread: SYSCONFIG
ti的工程师们你们好,我最近在做一个单相逆变器的相关应用需要用到锁相环,我看到solar库里面已经有单相sogi锁相环的功能,但是我对里面的应用步骤有一些疑问。
我打算使用CLA来运行solar库的spll_1ph_sogi函数,这里的第四步提到了逆变器的ISR运行最小频率要在20000Hz,我想请问这个逆变器的ISR运行最小频率是指的什么?是指我采样到的电压数据的采样频率吗?因为我原来的采样频率是5000Hz,我尝试将采样频率提升至20000Hz来运行,但是频率提升导致了我的储存数据点变成了原来的4倍,因此ccs里面build的过程中显示Description Resource Path Location Type
<a href="file:/C:/ti/ccs1220/ccs/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment/blocking fails for section ".bss" size 0x96e page 1. Available memory ranges: 2837xD_FLASH_lnk_cpu1.cmd /mytry_adc_led line 88 C/C++ Problem。(可能就是内存不足的意思吧)
因此我想问一下这个逆变器的ISR运行最小频率指的是什么?