一点load program,就出现以下报错:
CLA_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8000: Error 0x00000008/-2126 Error during: Break Point, FAIL TO SET SOFTWARE BREAKPOINT: This debug target does not support opcode replacement software breakpoints
CLA_0: Breakpoint Manager: Retrying with a Legacy Hardware breakpoint
CLA_0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x8b1b: Error 0x00000008/-2126 Error during: Break Point, FAIL TO SET SOFTWARE BREAKPOINT: This debug target does not support opcode replacement software breakpoints
CLA_0: Breakpoint Manager: Retrying with a Legacy Hardware breakpoint
CLA_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x8000: Failed to set one or more HW BPs. You may have exceeded the total number H/W breakpoints available. Disable one and try again. Please note that another module may have claimed one or more HW BPs.
CLA_0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x8b1b: Failed to set one or more HW BPs. You may have exceeded the total number H/W breakpoints available. Disable one and try again. Please note that another module may have claimed one or more HW BPs.
CLA_0: Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0x8000: Error 0x00000008/-2044 Error during: Break Point, No breakpoint at 0x00008000
点RUN 出现
an't Run Target CPU:
Error 0x00000020/-2060
Error during: Execution,
Processor is already running at 0x00000000
新手 求指导