常见问题,分几部分讨论(请大家补充)
1、怎么进行串口烧写
2、串口烧写碰到问题怎么办
3、TI提供哪些烧写方法
4、如何自行开发烧写方式
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
常见问题,分几部分讨论(请大家补充)
1、怎么进行串口烧写
2、串口烧写碰到问题怎么办
3、TI提供哪些烧写方法
4、如何自行开发烧写方式
上面发送的,41AA0800000000000000000000000000000000000000000800000000C011223344556677意思是
在0x0000c000写11223344556677
更具体的,可以参考bootROM文档中的说明:
关于有哪些烧写方法:
TI对于烧写芯片一般是这样建议的:
小于1000:用JTAG烧写或者通过串口烧写。M3,C2000没有类似于MSP430 GANG430这种工具,可能会有一些大型的烧写器,这里可以问问System General 和 XELTEK Inc ,他们出售这类工具。
或者下面这款,不过我没用测过。
elprotronic公司的flashpro2000
小于10000:联系负责你们的经销商或者专门的烧写公司烧写。比如:
• XELTEK, Inc
• System General
• Source Electronics
• BPM Microsystems
大于10000:联系TI定制芯片,让程序在芯片出厂的时候即已经固化在芯片中。
另外有很多第三方TI供各种烧入方法,串口,CAN....
最常见的是codeskin公司。。。
您好,我想请教一个问题,我用28335串口下载出现一个问题就是:
*** PLEASE RESET TARGET IN SCI BOOT-LOADER MODE ***
Connecting with target (autobaud)... failed (no response)!
不知道哪里错了
你好,我想问一下,假如我通过跳线帽引导为串口下载后,当我需要正常运行程序时,是否还得需要将硬件恢复原状才能正常运行啊?
您好,我当前用的是TMS320F2806,PCB板上晶振是25MHZ, 用codeskin,选择芯片为2806,频率选择20MHZ或27MHZ通过USB转串口进行程序烧写,程序我通过hex2000.exe转换了一个8位,和16位两个程序,进行烧写,结果如下:
*** PLEASE RESET TARGET IN SCI BOOT-LOADER MODE ***
Pinging target... Baudrate locked.
Bootloading... OK. Please wait...
Connecting with target... failed (no response)!
不过选择27MHZ能够更快的显示出“no reponse”
请问是何原因?,如何解决?