This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用EPWM控制ADC采样,双通道同步采样,如何提高采样率到2M到4M左右?

Other Parts Discussed in Thread: CONTROLSUITE

我的想法是采集两个通道的数据,采集1024个数据存入数组,然后再把数组中的数据输入显示屏,我设置的pwm频率为6.25MHZ,ADCCLK为12.5MHZ,采样率即为pwm的频率,可是实际测试结果的采样率只有300K左右,请大神指导一下,下面是我的程序。采样率的设置是在InitAdc1(void); InitEPwm1Example();ADC_cai(void);这三个子函数中

#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File

/**************************************宏定义************************************************/
#define DELAY_TIME_min 200 //延时时间(短)
#define DELAY_TIME_max 500000 //延时时间(长)
#define delay_short 300 // 10us
#define delay_long 300000 // 10ms
#define delay_mid 3000
#define SCIC 1
#define ADC_MODCLK 0x3 //ADC_MODCLK=HISPCP, HSPCLK = SYSCLKOUT/2*ADC_MODCLK = 150/(2*3)=25.0 MHz
/*****************************************************************************************************/

//串口C声明
void scic_loopback_init(void);
void scic_fifo_init(void);
void scic_xmit(int a);
void delay(Uint32 t);
void ADC_cai(void);

//串口相关变量
int j=0,w=0,y=0;//w用来设置等待adc采集,w=1表示采完结束。y表示一共执行adc采集中断子程序128次,共采到1024个点
char msg1[6]={0x5A,0xA5,0x05,0x82,0x10,0x05}; //Y_center相关指令
char msg2[6]={0x5A,0xA5,0x05,0x82,0x10,0x06}; //VD_center相关指令
char msg3[6]={0x5A,0xA5,0x05,0x82,0x10,0x09}; //横轴间隔设置相关指令
char msg4[6]={0x5A,0xA5,0x05,0x82,0x10,0x08}; //纵轴放大倍数设置相关指令
char msg[5]={0x5A,0xA5,0x04,0x84,0x01}; //写数据指令
char msg5[6]={0x5A,0xA5,0x03,0x80,0xEB,0x56};

int i=0;
int c_data; //要写的数据值
int c_data1,c_data2,c_data0;//中间转换参量
int dat_max,dat_mid,dat_min,mul;

/*************************************串口*********************************/
// Test 1,SCIC DLB, 8-bit word, baud rate 9.6k, default, 1 STOP bit, no parity

//该例中的全局变量:
Uint16 LoopCount;
Uint16 ConversionCount;
float Voltage1[1024]={0};
float Voltage2[1024]={0};
//unsigned int Voltage_1[100]={0};
//unsigned int Voltage_2[100]={0};
float Voltage_1[1024]={0};
float Voltage_2[1024]={0};
void InitAdc1(void);
void InitEPwm1Example();
volatile unsigned int adconvover=0;
interrupt void epwm1_timer_isr(void);//如果中断服务程序放在主函数的下面则在主函数前需要对中断服务程序进行声明,在主函数的上面则不需要。
Uint16 EPwm1TimerIntCount;
float a=4096;
float V2_max=0;
main()
{
int i,j;
InitSysCtrl(); //初始化系统函数
//InitGpio(); // 该例中跳过
InitScicGpio(); //选择GPIO口,初始化GPIO口
DINT;
IER = 0x0000; //禁止CPU中断
IFR = 0x0000; //清除CPU中断标志
InitPieCtrl(); //初始化PIE控制寄存器
InitPieVectTable(); //初始化PIE中断向量表
InitAdc1(); //初始化ADC模块
InitEPwm1Example();//初始化EPwm1模块
EnableInterrupts();
scic_fifo_init(); // Initialize the SCI FIFO
scic_loopback_init();
//服务程序
EALLOW; // This is needed to write to EALLOW protected register
//PieVectTable.ADCINT = &adc_isr;
SysCtrlRegs.HISPCP.all=ADC_MODCLK;//HISPCP=ADC_MODCLK, HISPCLK=SYSCLKOUT/2*HISPCP
PieVectTable.EPWM1_INT = &epwm1_timer_isr;
EDIS;
//开中断
PieCtrlRegs.PIEIER1.bit.INTx6=1;
PieCtrlRegs.PIEIER1.bit.INTx1=1;
PieCtrlRegs.PIEIER3.bit.INTx1 =0;//关PIE中断,EPWM-T1定时器中断位于INT3.1
IER |= M_INT3; //开CPU中断
EINT; // 使能全局中断
ERTM; // 使能实时中断
//epwm1_timer_isr();
// 等待ADC中断
// Initalize SCI
dat_max=2000;
dat_mid=1000;
dat_min=0;
mul=440.0*256/(dat_max-dat_min);

#if SCIC
//清屏
for (i=0;i<6;i++)
{
scic_xmit(msg5[i]);
delay(delay_short);
}
delay(delay_long);

delay(delay_long);
//修改VD-Center值
c_data=dat_mid;
c_data0=c_data;
c_data2=0xff&c_data0; // data2 为data的低八位数据
c_data0=c_data>>8;
c_data1=0xff&c_data0; // data1 为data的高八位数据
i = 0;
for (i=0;i<6;i++)
{
scic_xmit(msg2[i]);
delay(delay_short);
}
scic_xmit(c_data1);
delay(delay_short);
scic_xmit(c_data2);
delay(delay_short);
delay(delay_long);

delay(delay_long);

//修改纵轴放大倍数
c_data=mul;
c_data0=c_data;
c_data2=0xff&c_data0; // data2 为data的低八位数据
c_data0=c_data>>8;
c_data1=0xff&c_data0; // data1 为data的高八位数据
i = 0;
for (i=0;i<6;i++)
{
scic_xmit(msg4[i]);
delay(delay_short);
}
scic_xmit(c_data1);
delay(delay_short);
scic_xmit(c_data2);
delay(delay_short);
delay(delay_long);

delay(delay_long);
delay(delay_long);

//修改横轴间隔数
c_data=5;
c_data0=c_data;
c_data2=0xff&c_data0; // data2 为data的低八位数据
c_data0=c_data>>8;
c_data1=0xff&c_data0; // data1 为data的高八位数据
i = 0;
for (i=0;i<6;i++)
{
scic_xmit(msg3[i]);
delay(delay_short);
}
scic_xmit(c_data1);
delay(delay_short);
scic_xmit(c_data2);
delay(delay_short);
delay(delay_long);
while(ScicRegs.SCIFFTX.bit.TXFFST != 0);
#endif

ConversionCount = 0;
EPwm1TimerIntCount=0;

delay(delay_long);
while(1)
{
ADC_cai();

#if SCIC
for(j=0;j<1024;j++)
{

c_data=Voltage_2[j]*1000-100;
c_data0=c_data;
c_data2=0xff&c_data0; // data2 为data的低八位数据
c_data0=c_data>>8;
c_data1=0xff&c_data0; // data1 为data的高八位数据
i = 0;
for (i=0;i<5;i++)
{
scic_xmit(msg[i]);
delay(delay_short);
}
scic_xmit(c_data1);
delay(delay_short);
scic_xmit(c_data2);
delay(delay_short);

// ConversionCount++;
delay(delay_long);
}
//ConversionCount=0;
// delay(delay_long);

while(ScicRegs.SCIFFTX.bit.TXFFST != 0);
#endif

}
}

void InitEPwm1Example()
{
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;// 在系统初始化函数中已经使能
//EPWM模块,此处只需设置禁止同步。
EDIS;
//1.设置TB模块
EPwm1Regs.TBPRD =12; //18750 //2ms //设置计数周期=600TBCLK
//EPwm1Regs.TBPRD = 6000;
EPwm1Regs.CMPA.half.CMPA = 6; // 比较器A = 300TBCLK
//EPwm1Regs.CMPA.half.CMPA = 500;
EPwm1Regs.CMPB = 20; //比较器 B = 500 TBCLK
EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // 设置相位寄存器置零
EPwm1Regs.TBCTR = 0x0000; // 清除TB计数器

// Setup TBCLK = SYSCLKOUT / (HSPCLKDIV * CLKDIV)=150/4*4
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; //计数方式设置00 //Up-count mode;01Down-count mode;10 Up-down-count mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // 禁止相位加载
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; //从阴影寄存器加载计数值
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;//禁用同步输出,在头文
//件DSP2833x-ePwm-defines.h中有定义
EPwm1Regs.TBCTL.bit.HSPCLKDIV =TB_DIV1;//TB_DIV1=0
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;//TB_DIV1=0
EPwm1Regs.TBCTL.bit.FREE_SOFT = 0x3; //仿真模式位:自由运行

//设置比较模块
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; // 映射模式Load registers
//every ZERO
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR = Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

// 设置动作模块
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET;
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm1Regs.AQCTLB.bit.CBU = AQ_SET;
EPwm1Regs.AQCTLB.bit.CBD = AQ_CLEAR;

//事件触发子模块设置
//1.开始转换脉冲SOCA设置
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // 使能ADC开始转换A(EPWMxSOCA)脉冲 把1修改成了0,在ADC_cai()中再赋值1触发adc采集
EPwm1Regs.ETSEL.bit.SOCASEL = 4; //设置EPWMxSOCA何时生成,2,TBCTR=TBPRD
EPwm1Regs.ETPS.bit.SOCAPRD = 3; //第三个中断事件A发生,即EPWMxSOCA生成
//2.EPWM中断设置
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRD;//EPWM中断设置,此处设置为周期中断
EPwm1Regs.ETSEL.bit.INTEN = 1; //使能EPWM中断
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST;//第一个事件发生时产生中断

EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;// Enable TBCLK within the ePWM
EDIS;
}

void InitAdc1(void)
{
Uint16 i;

AdcRegs.ADCTRL1.bit.RESET=1; //复位AD 模块
for(i=0;i<9;i++)
{asm(" NOP");}
AdcRegs.ADCTRL1.bit.RESET=0;
AdcRegs.ADCTRL1.bit.SUSMOD=0; //仿真暂停方式,0为忽略。
AdcRegs.ADCTRL1.bit.ACQ_PS=0; //控制sSOC的脉冲宽度,同时也决定了采样开关闭合的时间。设定窗口大小SC=ADCTRL1[11:8] + 1 个ADCCLK周期数;

AdcRegs.ADCTRL1.bit.CPS=0; //内核时钟预定标器,1为二分频 ADC Core clock divider :HSPCLK/[2*(ADCTRL1[7]:CPS + 1)]
AdcRegs.ADCTRL1.bit.CONT_RUN=1;//连续运行方式,0:敉7绞?1:连续转换方式.
AdcRegs.ADCTRL1.bit.SEQ_CASC=1; //**级联蛄蟹⑸鞴ぷ鞣绞剑? 双序列模
//式;1 级联模式

//ADCTRL3对电源和采样方式进行设置
AdcRegs.ADCTRL3.bit.ADCBGRFDN=3;//带隙参考电路上电
for(i=0;i<10000;i++)
{asm(" NOP");}
AdcRegs.ADCTRL3.bit.ADCPWDN=1;//除带隙参考电路獾钠渌鸄DC模块上电
for(i=0;i<5000;i++)
{asm(" NOP");}
AdcRegs.ADCTRL3.bit.ADCCLKPS=2; // ADCCLK=HISPCLK/[2*ADCCLKPS*(ADCTRL1[7].CPS+1)]
AdcRegs.ADCTRL3.bit.SMODE_SEL=1; //采样方式。顺序采样0/同步采样1

AdcRegs.ADCMAXCONV.bit.MAX_CONV1=0x07; //设定转换数量,共8同步采样(每
//次采样两个通道),共采样16路
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; //采样ADCINA0和ADCINB0

AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x0; //采样ADCINA0和ADCINB0
AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 0x0; //采样ADCINA0和ADCINB0


//ADC状态和标志寄存器ADCST(清除中断标志)
AdcRegs.ADCST.bit.INT_SEQ1_CLR=1;//中断清除位
AdcRegs.ADCST.bit.INT_SEQ2_CLR=1;

//AdcRegs.ADCTRL2.all=0x2800;
AdcRegs.ADCTRL2.bit.EPWM_SOCB_SEQ=0;
AdcRegs.ADCTRL2.bit.RST_SEQ1=1;// 复位序列发生器1
//SEQ1
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1=0;//SEQ1中断使能:0禁止INT SEQ1向CPU发出中断申请,1使能INT SEQ1向CPU发出中断申请
AdcRegs.ADCTRL2.bit.INT_MOD_SEQ1=0;//SEQ1中断方式:0每个SEQ1序列转换 束,置位SEQ1的中断标志
AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1=1;//SEQ1的EPWM SOCA使能位,1使能
AdcRegs.ADCTRL2.bit.EXT_SOC_SEQ1=0;//SEQ1的外部SOC信号位,0:无操作。1:外部ADCSOC引脚信号启动ADC自动转换序列。
AdcRegs.ADCTRL2.bit.SOC_SEQ1=0;//为1时,软件启动ADC转换.
//SEQ2
AdcRegs.ADCTRL2.bit.RST_SEQ2=0; //复位SEQ2
AdcRegs.ADCTRL2.bit.SOC_SEQ2=0; //启动SEQ2的转换触发。仅适用于双序
//列发生器模式
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ2=0;
AdcRegs.ADCTRL2.bit.INT_MOD_SEQ2=0;
AdcRegs.ADCTRL2.bit.EPWM_SOCB_SEQ2=0;
}

void ADC_cai(void)
{
AdcRegs.ADCTRL2.bit.RST_SEQ1=1;
AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;
PieCtrlRegs.PIEACK.all|=0x0001;
PieCtrlRegs.PIEIER1.bit.INTx1=0;
for(i=0;i<5000;i++)
{asm(" NOP");}
w=0;
PieCtrlRegs.PIEIER1.bit.INTx6=0;//控制ADC中断
// delay(DELAY_TIME_min);
AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;//为1时,软件启动ADC转换//为1时,软件启动ADC转换
//PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // 使能ADC开始转换A(EPWMxSOCA)脉冲
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
//EPwm1Regs.ETCLR.bit.INT = 1;
EPwm1Regs.ETSEL.bit.INTEN = 1;//使能ePWM中断产生位;1:使能中断;0:禁止中断

loop: if(w==0)
{
goto loop;
}

// delay(DELAY_TIME_max);
PieCtrlRegs.PIEIER1.bit.INTx6=1;
PieCtrlRegs.PIEIER1.bit.INTx1=1;
}

//EPWM1的定时器中断
interrupt void epwm1_timer_isr(void)
{

AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;//向该位写1,清除SEQ1中断标志位,INT_SEQ1,该位对EOS_BUF1位无影响。
//AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;//为1时,软件启动ADC转换//为1时,软件启动ADC转换
PieCtrlRegs.PIEACK.all |= PIEACK_GROUP1;

Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT0 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT1 >>4)*3.0/4096.0;

ConversionCount++;
// Voltage_1[ConversionCount] = AdcRegs.ADCRESULT2;
Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT2 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT3 >>4)*3.0/4096.0;
ConversionCount++;
//Voltage_1[ConversionCount] = AdcRegs.ADCRESULT4 ;
Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT4 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT5 >>4)*3.0/4096.0;
ConversionCount++;

Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT6 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT7 >>4)*3.0/4096.0;
ConversionCount++;

Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT8 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT9 >>4)*3.0/4096.0;
ConversionCount++;

Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT10 >>4)*3.0/4096.0;

Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT11 >>4)*3.0/4096.0;
ConversionCount++;
Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT12 >>4)*3.0/4096.0;
Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT13 >>4)*3.0/4096.0;
ConversionCount++;
Voltage_1[ConversionCount] = (AdcRegs.ADCRESULT14 >>4)*3.0/4096.0;
Voltage_2[ConversionCount] =( AdcRegs.ADCRESULT15 >>4)*3.0/4096.0;

ConversionCount++;
//y++;
if(ConversionCount> 1023)
{
ConversionCount = 0;
w=1;
//y=0;
//ConversionCount = 0;
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;//复位SEQ1为初始状态 CONV00
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1=1;
PieCtrlRegs.PIEIER3.bit.INTx1 = 0;//使能PIE中断,EPWM-T1定时器中断位于INT3.1
EPwm1Regs.ETSEL.bit.INTEN = 0;//使能ePWM中断产生位;1:使能中断;0:禁止中断
//AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1=0;
// AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;
PieCtrlRegs.PIEACK.all= PIEACK_GROUP3;
EPwm1Regs.ETCLR.all = 0xD;//epwm中断标准清除位,0:没有效果;1:清除中断标志位
// AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit,清除INT SEQ1标志位

}

else
{
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
EPwm1Regs.ETCLR.bit.INT = 1;
// AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1;
//PieCtrlRegs.PIEIER3.bit.INTx1 = 1;

//EPwm1Regs.ETSEL.bit.INTEN = 1;//使能ePWM中断产生位;1:使能中断;0:禁止中断

PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
// AdcRegs.ADCTRL2.bit.SOC_SEQ1=1;//为1时,软件启动ADC转换//为1时,软件启动ADC转换
 }

}
void scic_loopback_init()
{
// Note: Clocks were turned on to the SCIC peripheral
// in the InitSysCtrl() function

ScicRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
ScicRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
ScicRegs.SCICTL2.all =0x0003;
ScicRegs.SCICTL2.bit.TXINTENA =1;
ScicRegs.SCICTL2.bit.RXBKINTENA =1;
ScicRegs.SCIHBAUD =0x0001;
ScicRegs.SCILBAUD =0x00e7;
ScicRegs.SCICCR.bit.LOOPBKENA =0;// enable loop back
ScicRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}


// Transmit a character from the SCI'
void scic_xmit(int a)
{
ScicRegs.SCITXBUF=a;
}

// Initalize the SCI FIFO
void scic_fifo_init()
{
ScicRegs.SCIFFTX.bit.TXFIFOXRESET=0;
ScicRegs.SCIFFRX.bit.RXFIFORESET=0;
ScicRegs.SCIFFTX.all=0xE040;
ScicRegs.SCIFFRX.all=0x204f;
ScicRegs.SCIFFCT.all=0x0;
}

void delay(Uint32 t)
{
Uint32 i = 0;

for (i = 0; i < t; i++);
}