The function: DCLINK_SS_runFastPWMCompensation(); 。in the file ''dclink_ss.h'' of the foc example of single resistor sampling, there seems to be an error, in the When vecArea = 3, the direction of movement seems to be reversed, the comment is written in the right direction, but the code direction is reversed.
您好
DCLINK_SS_runFastPWMCompensation() is not recommended to use for single shunt. It's not tested.