This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36P63C的ADC端口内阻是多大?



各位专家好,

    1、 我用的MCU是F28M36P63C,请问这款芯片的ADC端口内阻是多大?或者范围是多大?

    2、在AD端口外部采用电阻分压来测量某一电压时,在阻值选取时,需要有什么注意的?

    3、如果在AD端口外部设置一个RC滤波电路,请问R在选值时有何考量?R与AD端口内阻有何匹配关系?

    4、是否有必要在AD端口外部增加一个电压跟随器?

  • 1、对地的内阻是很大的,具体值不清楚

    2、电阻分压的话,需要考虑电阻功耗。另外就是到ad输入口的电压不能超过允许范围。

    3、RC滤波主要考虑的是时间常数,内阻我觉得还是可以不考虑。

    4、一般会添加,如果应用场合一般,只是做个小实验也可以不用

  • 你好     1.ADC接口是高阻   也就是在采样的时候不能影响到你的接入电压

    2.分压电阻个人觉得你只需要考虑两个电阻流过的电流就可以啦

    3.RC滤波器只要能满足你的滤波效果就好

    4.电压跟随作用不是很大   但是钳位电路个人觉得很有必要