Part Number: TMS320F28388D
我在vcu2_crc.h文件里看到有CRC_reset函数的声明。C2000库里面的libraries/dsp/VCU/c28/source/vcu2/crc路径下的vcu2_crc_utils.asm文件里是不是需要添加对CRC_reset的登记?下面是我补充后的样子,添加在了macro段落。
;;*****************************************************************************
;;! \file source/vcu2/vcu2_crc_utils.asm
;;!
;;! \brief 8-bit CRC
;;#############################################################################
;;!
;;! Copyright: Copyright (C) 2023 Texas Instruments Incorporated -
;;! All rights reserved not granted herein.
;;! Limited License.
;;!
;;! Texas Instruments Incorporated grants a world-wide, royalty-free,
;;! non-exclusive license under copyrights and patents it now or hereafter
;;! owns or controls to make, have made, use, import, offer to sell and sell
;;! ("Utilize") this software subject to the terms herein. With respect to the
;;! foregoing patent license, such license is granted solely to the extent that
;;! any such patent is necessary to Utilize the software alone. The patent
;;! license shall not apply to any combinations which include this software,
;;! other than combinations with devices manufactured by or for TI
;;! ("TI Devices").
;;! No hardware patent is licensed hereunder.
;;!
;;! Redistributions must preserve existing copyright notices and reproduce this
;;! license (including the above copyright notice and the disclaimer and
;;! (if applicable) source code license limitations below) in the documentation
;;! and/or other materials provided with the distribution.
;;!
;;! Redistribution and use in binary form, without modification, are permitted
;;! provided that the following conditions are met:
;;!
;;! * No reverse engineering, decompilation, or disassembly of this software is
;;! permitted with respect to any software provided in binary form.
;;! * Any redistribution and use are licensed by TI for use only
;;! with TI Devices.
;;! * Nothing shall obligate TI to provide you with source code for the
;;! software licensed and provided to you in object code.
;;!
;;! If software source code is provided to you, modification and redistribution
;;! of the source code are permitted provided that the following conditions
;;! are met:
;;!
;;! * any redistribution and use of the source code, including any resulting
;;! derivative works, are licensed by TI for use only with TI Devices.
;;! * any redistribution and use of any object code compiled from the source
;;! code and any resulting derivative works, are licensed by TI for use
;;! only with TI Devices.
;;!
;;! Neither the name of Texas Instruments Incorporated nor the names of its
;;! suppliers may be used to endorse or promote products derived from this
;;! software without specific prior written permission.
;;#############################################################################
;;
;;*****************************************************************************
;;
;;*****************************************************************************
;; includes
;;*****************************************************************************
;;
;;*****************************************************************************
;; global defines
;;*****************************************************************************
;; CRC Routine defines
;;*****************************************************************************
;; macros 2025.05.12
;;*****************************************************************************
.if $defined(__TI_EABI__)
.if __TI_EABI__
.asg CRC_reset, _CRC_reset
.endif
.endif
;;*****************************************************************************
;; globals
;;*****************************************************************************
.global _CRC_reset
;;*****************************************************************************
;; function definitions
;;*****************************************************************************
.text
;; \brief Workaround to the silicon issue of first VCU calculation on power up being
;; erroneous
;;
;; Details Due to the internal power-up state of the VCU module, it is possible
;; that the first CRC result will be incorrect. This condition applies to the
;; first result from each of the eight CRC instructions.
;; This rare condition can only occur after a power-on reset, but will not
;; necessarily occur on every power on. A warm reset will not cause this condition
;; to reappear.
;; Workaround(s) The application can reset the internal VCU CRC logic by
;; performing a CRC calculation of a single byte in the initialization routine.
;; This routine only needs to perform one CRC calculation and can use any of the
;; CRC instructions
;;
;;
_CRC_reset:
MOVB XAR7, #0
VCRC8L_1 *XAR7
VCRCCLR
LRETR
;; End of file