太阳能微型逆变器套件中,在没有MPPT的情况下,前级DC-DC侧给定个参考电流Ipv_ref,根据检测Ipv值,通过一个2P2Z的调节器,产生PWM,如果我要DC-AC工作的话,假设是并到220v的电网,那我的逆变开启电压要380v;怎么能保证我达到了Ipv_ref时,就有个380v电压的输出;给的实验步骤中给的Ipv_ref是0.1,可以通过调节得到个380v电压,那我要是给个Ipv_ref等于0.2,能不能得到380v呢?它这个工作的原理不明白,不知道有没有说清楚,附上原理图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢你的答复!如果给的参考电流1A,这个时候通过2P2Z调节器可以得到一个占空比,使输出电压达到380v,那我给个2A的参考电流,这个时候产生的占空比理论上就参考电流1A的时候得到的占空比要大,那这个时候我的输出电压应该大于380v,逆变是有个过电压和欠电压保护,可是输出电压大于380v时,占空比就设置成0了,这个过程该怎么理解呢?谢谢