This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 关于PGA_GND的连接问题

Part Number: TMS320F280049C


刚开始学习C2000,现在在根据官方数据手册绘制核心板时,遇到一些困惑的点,如下:
PGA_GND理想设计应该是开尔文连接,这里的开尔文连接指的是什么,我可否直接接在核心板上的GND(连接的VSSA、VSS、VREFLOA、VREFLOB、VREFLOC)。

还有PGA_IN的端口在不使用的时候应该连接到VSS还是悬空即可。

在连接VREFHIB\VREFHIC和VREFHIA这两个ADC外置参考源时,我将这两个端口连接在一起,并连接2.2uF的陶瓷电容,接到REF3030外置参考源上,这种设计是否有问题,还是应该
将VREFHIB\VREFHIC端口和VREFHIA分开连接到REF3030参考源,同时2个端口上都连接2.2uF的陶瓷电容。

谢谢!