This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片为RM42,主频100M。
前期发现在调用F021 API 进行模拟EEPROM写入操作时会引起nERROR引脚动作。
经过调查简化,发现在main中一开始只要调用Fapi_initializeFlashBanks(100)之后,即会触发ESM故障,查看ESMSR3得知发生了Group3 Channel7故障,解释为:
FMC - uncorrectable. bu1 and bu2 interfaces.....
请问这个问题应该怎么解决
Deli 你好,
1. 如果你使用BANK7 for EEPROM,你直接调用EEPROM的API就可以。不需要另外调用Fapi_initializeFlashBanks(..) function。 请用HALCOGEN产生EEPROM的drivers,再用EEPROM的例程测试。
2. 如果您用在一般的flash,请参照RM42的bootloader。bootloader中的flash.c用flash的使用例程。
Regards,
Qingjun