我对该程序的理解是MIBSPI自收自发,以TG0~TG3依次软件触发,TG0的收发完成触发TG1的收发,依次类推,但问题是DEBUG结束一直停留在wait的地方,观察RXDATA数组也没有收到数据,不知道哪里的问题,硬件上需要做什么连接吗? 程序如下:
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
#include "sys_core.h"
#include "mibspi.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
uint16 TG0_TX_DATA[8] = {0x1000, 0x1111, 0x1222, 0x1333, 0x1444, 0x1555, 0x1666, 0x1777};
uint16 TG0_RX_DATA[8]= {0};
uint16 TG1_TX_DATA[8] = {0x2000, 0x2111, 0x2222, 0x2333, 0x2444, 0x2555, 0x2666, 0x2777};
uint16 TG1_RX_DATA[8]= {0};
uint16 TG2_TX_DATA[8] = {0x3000, 0x3111, 0x3222, 0x3333, 0x3444, 0x3555, 0x3666, 0x3777};
uint16 TG2_RX_DATA[8]= {0};
uint16 TG3_TX_DATA[8] = {0x4000, 0x4111, 0x4222, 0x4333, 0x4444, 0x4555, 0x4666, 0x4777};
uint16 TG3_RX_DATA[8]= {0};
uint32_t TG3_IS_Complete;
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
TG3_IS_Complete = 0x55555555;
/* Enable IRQ Interrupt in Cortex R4 CPU */
_enable_interrupt_();
/* - initializing mibspi - enabling tg 0,1,2,3 , length 8 bytes each
* TG 0 - Configured for TICK Trigger
* TG 1, 2, 3, are SOftware Triggered
* CS 0 is used. - CS0 is in HOLD Mode,
* CS 0 Toggles only after Each TG ( Every 8 byte) is complete
* Trigger is One Shot, so only once the TG will transmit.
*/
mibspiInit();
/* - enabling loopback ( this is to emulate data transfer without external wires */
mibspiEnableLoopback(mibspiREG1,Digital_Lbk);
/* Enable TG 0,1,2,3 complete interrupt to INT 0 */
mibspiEnableGroupNotification(mibspiREG1,0,0);
mibspiEnableGroupNotification(mibspiREG1,1,0);
mibspiEnableGroupNotification(mibspiREG1,2,0);
mibspiEnableGroupNotification(mibspiREG1,3,0);
/* Fill the transfer Groups */
mibspiSetData(mibspiREG1,0,TG0_TX_DATA);
mibspiSetData(mibspiREG1,1,TG1_TX_DATA);
mibspiSetData(mibspiREG1,2,TG2_TX_DATA);
mibspiSetData(mibspiREG1,3,TG3_TX_DATA);
/* Enable TG0 to start, once tickCNT triggers */
mibspiTransfer(mibspiREG1,0);
/* Configure TICKCNT
* DATA FORMAT 0 is selected which has *** set as 1000KHz
* So tick is 0xFFFF * (1/1000KHz) = 65.5535 msec*/
mibspiREG1->TICKCNT = 0x8000FFFF;
/* Wait until this flag is set in TG3 ISR */
while(TG3_IS_Complete != 0xA5A5A5A5);
mibspiGetData(mibspiREG1,0,TG0_RX_DATA);
mibspiGetData(mibspiREG1,1,TG1_RX_DATA);
mibspiGetData(mibspiREG1,2,TG2_RX_DATA);
mibspiGetData(mibspiREG1,3,TG3_RX_DATA);
while(1);
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
void mibspiGroupNotification(mibspiBASE_t *mibspi, uint32 group)
{
switch (group){
case 0 :
/* Enable TG1 to start, SW Trigger */
mibspiTransfer(mibspiREG1,1);
break;
case 1 :
/* Enable TG1 to start, SW Trigger */
mibspiTransfer(mibspiREG1,2);
break;
case 2 :
/* Enable TG1 to start, SW Trigger */
mibspiTransfer(mibspiREG1,3);
break;
case 3 :
/* Enable TG0 to start, SW Trigger */
//mibspiTransfer(mibspiREG1,0);
TG3_IS_Complete = 0xA5A5A5A5;
break;
default :
while(1);
break;
}
}
/* USER CODE END */
希望得到指导谢谢!