This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952(D)ZWTT访问SDRAM错误求助



在使用MemCopy命令对外挂SDRAM(容量128MB)进行访问时出现错误,通过时序抓取发现操作时发生了Burst执行被打断,如通过MemSet将4个字节进行清零后用Memcopy写入值这一操作,在MemSet未执行完就进行了写操作,仅将第一个字节写入后又回来执行MemSet,执行完成后再次通过MemCopy进行写入,在MemSet第一次被打断时地址就发生了紊乱,结果表现为将后三个字节的内容写入了前三个字节的地址中,整个软件应用中未开启中断,在MemSet和MemCopy指令之间插入其他无效代码(如延时)后会影响结果,例如延时1ms就不出现此故障。将EMIF总线频率从110MHz降到55MHz,故障现象依旧,降到44MHz后故障不在此处出现,为了验证是否故障已得到解决,对所有地址进行写入后再读出比较,发现总线控制器仍会在其他地方出现紊乱,例如从地址0x4FC跳过0x4FE直接操作0x500地址等故障现象,降频至36MHz后为再出现上述故障现象。现有两个疑问:1、出现此故障的原因是什么(硬件设计时已充分考虑了阻抗匹配、等长匹配等信号完整性设计,且总线控制器紊乱并非在某次操作仅某一位地址线状态翻转)?;2、在技术文档“ZHCS441B”第93页中定义tc(clk)最低18ns,而文档“SPNU503B”第609页中进行SDRAM的RR时间计算时以100MHz在进行举例,对外挂SDRAM进行操作时EMIF时钟最大应为多少?