This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952(D)ZWTT无法正常工作求助

在几百片ARM中出现了如下几种芯片无法正常工作的情形:1、有两张生产回来的板卡,短路、断路测试无故障,上电下载好代码后,指示灯指示正常后断电保存,第二天入库检查,发现模块只亮电源灯,经测试3.3V电源网络阻抗异常,大约10Ω左右(正常情况大于100Ω),ARM芯片发烫严重;2、有一张板卡老化试验之前模块正常运行,单板测试正常,50℃运行96小时后模块异常,只亮电源灯,进行单板测试发现3.3V电源网络阻抗异常,约10Ω左右,ARM芯片无异常发热情况;3、生产回来的一张板卡在下载好代码后,指示灯均正常指示,然后断电保存,第二天模块上电进行测试时发现异常,3.3V电源网络对地阻抗基本没太大变化,但ARM上电复位管脚无法上拉到3.3V,只有1.6V左右,无法下载程序,通过外部强行上拉到3.3V也无法下载程序,当重新恢复10k上拉电阻后,此复位管脚能上拉到3.17V左右(猜测此管脚内部已经断线?),仍无法通过JTAG下载程序;4、一张生产回来的板卡在下载好代码后,指示灯均正常指示,然后断电保存,第二天模块上电进行测试时异常,ARM内部3.3V对地短路,阻抗为0Ω左右;5、两张生产回来的板卡,经短路、断路测试正常后进行上电,模块通过JTAG下载代码失败,对板卡进行单板测试,ARM芯片的供电正常,电源网络对地阻抗正常,时钟正常,复位管脚输入电平正常,目测电路板焊接正常,JTAG端口所有信号和其他正常板卡电平状态一致,两张板卡中一张的nERROR管脚输出为低电平,另一张输出为高电平。能否针对上述几类故障情形大致分析可能原因呢?