This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48 Boodloader linker for keil

各位前輩好:

小弟最近移值官網的HDK BootLoader Sample Code 到keil C 開發環境,在linker 檔遇到問題,問題如下:

下面是CCS  bl_link.cmd 資料

--retain="*(.intvecs)"

MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000014E0
FLASH0 (RX) : origin=0x00001500 length=0x002FEB00 //LS31x Flash size is 0x300000
SRAM (RW) : origin=0x08002000 length=0x0002D000
STACK (RW) : origin=0x08000000 length=0x00002000
}
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
..\Debug\Fapi_UserDefinedFunctions.obj (.text)
..\Debug\bl_flash.obj (.text)

--library= I:\CCS_Test\SafetyMCU_Bootloader\lib\F021_API_CortexR4_LE.lib < FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.SetActiveBank.obj
FlashStateMachine.InitializeFlashBanks.obj
FlashStateMachine.EnableMainSectors.obj
FlashStateMachine.IssueFsmCommand.obj
FlashStateMachine.ScaleFclk.obj
Init.obj
Utilities.CalculateEcc.obj
Utilities.WaitDelay.obj
Utilities.CalculateFletcher.obj
Read.MarginByByte.obj
Read.Common.obj
Read.FlushPipeline.obj
Read.WdService.obj
Async.WithAddress.obj
Program.obj > (.text)
} load = FLASH_API, run = SRAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)

.text > FLASH0
.const > FLASH0
.cinit > FLASH0
.pinit > FLASH0
.data > SRAM
.bss > SRAM
}

SECTIONS的這段code該怎麼移值到keil C 的,目前下面是我的設定,不過SECTIONS部份還沒辦法移值過來,compiler 出來的map檔跟CCS在FLASH_API段不一樣。

FLASH 0x00000000 0x00300000
{
 VECTORS 0x00000000 0x00000020
 {
 *.o (intvecs, +First)
 }
 FLASH_API 0x00000020 0x000044E0
 {
 *(+RO)
 }
 FLASH0 0x00004500 0x002FEB00
 {
 .ANY2 (+RO)
 }
 SRAM 0x08002000 0x0002D000
 {
 *.o (.data, +ZI +RW)
*.o (.bss)
 .ANY (+ZI +RW)
 }
 STACK 0x08000000 0x00002000
 {
 .ANY (+RW)
 }

有沒有人有這方面的經驗可以分享的,謝謝! 

  • 不清楚,不知道他们的编译器通用不通用。并不是所有的都通用的。比如编译51Keil编译器,就跟编译ARM的keil编译器不同。还是按照官方指定的开发工具做吧

  • 有人知道下面這三段code在做什麼?

    /* initalise copy table */
    if ((unsigned *)&__binit__ != (unsigned *)0xFFFFFFFF)
    {
        extern void copy_in(void *binit);
        copy_in((void *)&__binit__);
    }

    /* initalise the C global variables */
    if (&__TI_Handler_Table_Base < &__TI_Handler_Table_Limit)
    {
        unsigned char **tablePtr = (unsigned char **)&__TI_CINIT_Base;
        unsigned char **tableLimit = (unsigned char **)&__TI_CINIT_Limit;

        while (tablePtr < tableLimit)
        {
            unsigned char *loadAdr = *tablePtr++;
            unsigned char *runAdr = *tablePtr++;
            unsigned char idx = *loadAdr++;
            handler_fptr handler = (handler_fptr)(&__TI_Handler_Table_Base)[idx];

            (*handler)((const unsigned char *)loadAdr, runAdr);
        }
    }

    /* initalise contructors */
    if (__TI_PINIT_Base < __TI_PINIT_Limit)
    {
        void (**p0)() = (void *)__TI_PINIT_Base;

        while ((unsigned)p0 < __TI_PINIT_Limit)
        {
            void (*p)() = *p0++;
            p();
        }
    }

    -------------------------------------------------------------------------

    /* initalise the C global variables */
    if (&__TI_Handler_Table_Base < &__TI_Handler_Table_Limit)
    {
        unsigned char **tablePtr = (unsigned char **)&__TI_CINIT_Base;
        unsigned char **tableLimit = (unsigned char **)&__TI_CINIT_Limit;

        while (tablePtr < tableLimit)
        {
            unsigned char *loadAdr = *tablePtr++;
            unsigned char *runAdr = *tablePtr++;
            unsigned char idx = *loadAdr++;
            handler_fptr handler = (handler_fptr)(&__TI_Handler_Table_Base)[idx];

            (*handler)((const unsigned char *)loadAdr, runAdr);
        }
    }

    這段code還會跑copy_decompress_lzss.c的下面這段code

     

    /*****************************************************************************/

    /*                                                                           */

    /* __TI_DECOMPRESS_LZSS() - Decompress data encoded using LZSS encoding.     */

    /*                          Input buffer (inbuf) has the encoded data and    */

    /*                          uncompressed data is returned in outbuf.         */

    /*                                                                           */

    /*****************************************************************************/

    __attribute__((section(".text:decompress:lzss")))

    void __TI_decompress_lzss(pointer_to_const_t inbuf, pointer_t outbuf)

    {

        while (1)

        {

            flags_t flags = READ_CHAR_ADV(inbuf);

     

            int i;

            for (i=0; i<CHAR_BIT ; i++)

            {

               if (flags & 0x1)

               {

                  /*---------------------------------------------------------------*/

                  /* We have an uncoded byte, just write it out.                   */

                  /*---------------------------------------------------------------*/

                  WRITE_CHAR_ADV(outbuf, READ_CHAR_ADV(inbuf));

               }

               else

               {

                  /*---------------------------------------------------------------*/

                  /* Read and unpack the offset and length                         */

                  /*---------------------------------------------------------------*/             

                  offset_t offset;

                  length_t length;

    #if CHAR_BIT == 8

                  offset = READ_CHAR_ADV(inbuf);

                  length = READ_CHAR_ADV(inbuf);

                  offset <<= 4;

                  offset |= ((length & 0x00F0) >> 4);

                  length = (length & 0x000F) + 3;

                  /*---------------------------------------------------------------*/

                  /* If the length is 3->17, we only use 4 bits. If the length is  */

                  /* >= 18, we read an additional 8 bits and add it to the length. */

                  /*                                                               */

                  /* If the msb of the second byte is 1, we read an additional     */

                  /* 8 bits and use that for bits 7-14 of the length. This gives   */

                  /* us a range of 3->32785.                                       */

                  /*---------------------------------------------------------------*/

                  if (length == 18)

                  {

                     length_t length2 = READ_CHAR_ADV(inbuf);

                     if (length2 & 0x80)

                     {

                        length_t length3 = READ_CHAR_ADV(inbuf);

                        length2 = (length2 & 0x7f) | (length3 << 7);

                     }

                     length += length2;

                  }

    #elif CHAR_BIT == 16

                  unsigned char temp = READ_CHAR_ADV(inbuf);

                  length = (temp & 0xf) + 2;

                  offset = temp >> 4;

     

                  /*---------------------------------------------------------------*/

                  /* If the length is the maximum value encoded in 4 bits, read an */

                  /* additional 16-bit value and add it to the length.             */

                  /*---------------------------------------------------------------*/             

                  if (length == 17)

                     length += READ_CHAR_ADV(inbuf);

    #endif

                  /*---------------------------------------------------------------*/

                  /* If the offset indicates end of data, exit.                    */

                  /*---------------------------------------------------------------*/

                  if (offset == LZSS_EOD)

                     return;          

                  /*---------------------------------------------------------------*/

                  /* Copy the decoded string from sliding window to output buffer. */

                  /*---------------------------------------------------------------*/

                  length_t j;

                  pointer_t pos = outbuf - offset - 1;

                  for (j = 0; j < length; j++)

                     WRITE_CHAR_ADV(outbuf, READ_CHAR_ADV(pos));

               }

               flags >>= 1;

            }

        }

    }