_c_int00
if ((esmREG->SR1[2]) != 0U)   //  esmREG->SR1[2] == 2, 进入下面的for。
 {
/* USER CODE BEGIN (24) */
/* USER CODE END */
 /*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
 /*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
 /*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
 for(;;)
 { 
 }/* Wait */
这是什么原因引起的?
谢谢