Other Parts Discussed in Thread: ISO1050, ISO1042
两片TMS570,一片做冷备不加电,两片的Can通信口通过各自的TJa1040后直接连在了一起,与外部通信。现在加电工作的570的Can线上的电压返回到了不加电的570上,测量其MIBSPI口有1V左右电压输出,请问如何解决
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Leonardo,
建议加隔离CAN收发器,例如ISO1042, ISO1050.
The ISO1042 device is a galvanically-isolated controller area network (CAN) transceiver that meets the specifications of the ISO11898-2 (2016) standard. The ISO1042 device offers ±70-V DC bus fault protection and ±30-V common-mode voltage range. The device supports up to 5-Mbps data rate in CAN FD mode allowing much faster transfer of payload compared to classic CAN. This device uses a silicon dioxide (SiO2) insulation barrier with a withstand voltage of 5000 VRMS. Used in conjunction with isolated power supplies, the device prevents noise currents on a data bus or other circuits from entering the local ground and interfering with or damaging sensitive circuitry. The ISO1042 device is available for both basic and reinforced isolation (see Reinforced and Basic Isolation Options).
ISO1050 是一款电镀隔离的 CAN 转发器,此转发器符合或者优于 ISO11898-2 标准的技术规范。 此器件有几个由氧化硅 (SiO2) 绝缘隔栅分开的逻辑输入和输出缓冲器,此绝缘隔栅为说明第一段中的ISO1050DW 和针对 ISO1050DUB 的 2500 VRMS。 与隔离式电源一起使用,此器件可防止数据总线或者其它电路上的噪音电流进入本地接地并干扰和损坏敏感电路。
作为 CAN 收发器,该器件可为总线和 CAN 控制器分别提供差分发射能力和差分接收能力,信号传输速率高达 1 兆位每秒 (Mbps)。 该器件尤其适合工作在恶劣环境下,其具有串线、过压和接地损耗保护(–27V 至 40V)以及过热关断功能,共模电压范围为–12V 至 12V。