1.RM48L952和XRM48952的区别是什么,
2.XRM48952是否可以下单
如下图是命名规则,我不明白为什么不合格的也有料号,这个可以下单吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.RM48L952和XRM48952的区别是什么,
2.XRM48952是否可以下单
如下图是命名规则,我不明白为什么不合格的也有料号,这个可以下单吗
您好,
关于型号前缀的区别在甄误表中有给出:
http://www.ti.com.cn/cn/lit/er/spnz223b/spnz223b.pdf
X — Experimental device that is not necessarily representative of the final device's electrical
specifications.
P — Final silicon die that conforms to the device's electrical specifications but has not completed quality
and reliability verification.
NULL — Fully-qualified production device.
X and P devices are shipped against the following disclaimer:
"Developmental product is intended for internal evaluation purposes."
Production devices have been characterized fully, and the quality and reliability of the device have been
demonstrated fully. TI's standard warranty applies.Predictions show that prototype devices (X or P) have a greater failure rate than the standard production devices. Texas Instruments recommends that these devices not be used in any production system because their expected end-use failure rate still is undefined. Only qualified production devices are to be used.
Hi Hank,
带x的并非不合格的产品,一般为工程样品,作为前期产品内部开发及评估使用。而你下单的话,建议选择RM48L952产品.