TMS570LS3137是固定的大端格式吗?怎么修改成小端格式啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Wenyuan,
Hercules 产品目前常用的有两个系列,一个是TMS570系列,一个是RM系列。其中TMS570LS3137为大端格式,RM为小端格式。你是应用在什么场合?如果不需要某些特定车载总线或不需要过ISO26262功能安全等,也可以考虑一下RM系列。
1. RM4X 主要用于工业医疗, 产品有48系列,46系列,42系列。 其中48系列主频最快,可达220M, 42系列主频可达80M。RM4x为小端模式(Little-endian)。
2. TMS570 主要应用于汽车领域,产品符合IEC61508工业标准和ISO26262汽车标准。产品系列分别有0432,L1,L3,12x等系列,其中L3系列相当于RM4X中的48系列,主频可达180M, 12x系列相当于RM4x的46系列,主频可达160M,其中ZWT封装主频可达180M,0432相当于RM4x的42系列,主频可达80M。TMS570为大端模式(big-endian),即数据的高字节,保存在内存的低地址中,而数据的低字节,保存在内存的高地址中。这样的存储模式有点儿类似于把数据当作字符串顺序处理:地址由小向大增加,而数据从高位往低位放;
3. TMS470 是Cortex-M3的核, 体积小,价格便宜,支持IEC61508标准。
RM57和TMS570LC43是最新产品,主频可达350M