This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[2135 CAN]请协助分析并定位CAN通信问题

Other Parts Discussed in Thread: TMS570LS2135, HALCOGEN

1、问题现象:

CAN接口不能正常发送CAN消息,MCU CAN引脚到CAN Transceiver使用示波器不能抓取到正确的波形。最终收发器也不能正常发送出去波形。

 

2、MCU:TMS570LS2135 PGE封装

3、CAN接口逻辑电路设计:

 

CAN收发器相关设计(如下为CAN1的收发器,与上稍有差异)

 

 

 

3、Halcogen设置:

1)Halcogen上仅使能CAN1和CAN2 Driver

2)设置CAN2邮箱,仅测试MessageBox1,波特率设置500Kbps

 

4 测试代码:仅在sysmain中使用如下代码:

 

5、单步跟踪发送函数后其寄存器的值如下:

Ctrl       0x00031402    Config register [Memory Mapped]           

ErrStat 0x00000007    Status register [Memory Mapped]           

ErrCnt  0x00000000    Error Counter Register [Memory Mapped]         

Btr        0x00001453    Bit Timing_BRP Extension Register [Memory Mapped]       

IntR      0x00000000    Interrupt Register [Memory Mapped]           

Test     0x00000080    Test Register [Memory Mapped]           

ParErr  0x00000140    Parity Error Code Register [Memory Mapped]         

Rel       0xA3170504    Core Release Register [Memory Mapped]         

AboT    0x00000000   Auto Bus On Time [Memory Mapped]           

TrReqX            0x00000000    Transmission Request X [Memory Mapped]       

TrReq12          0x00000000    Transmission Request 2-1 [Memory Mapped]       

TrReq34          0x00000000    Transmission Request 4-3 [Memory Mapped]       

TrReq56          0x00000000    Transmission Request 6-5 [Memory Mapped]       

TrReq78          0x00000000    Transmission Request 8-7 [Memory Mapped]       

NewDatX         0x00000000    New Data X [Memory Mapped]         

NewDat12        0x00000000    New Data 2-1 [Memory Mapped]         

NewDat34        0x00000000    New Data 4-3 [Memory Mapped]         

NewDat56        0x00000000    New Data 6-5 [Memory Mapped]         

NewDat78        0x00000000    New Data 8-7 [Memory Mapped]         

IntPenX           0x00000000    Interrupt Pending X [Memory Mapped]         

IntPen12          0x00000000    Interrupt Pending 2-1 [Memory Mapped]       

IntPen34          0x00000000    Interrupt Pending 4-3 [Memory Mapped]       

IntPen56          0x00000000    Interrupt Pending 6-5 [Memory Mapped]       

IntPen78          0x00000000    Interrupt Pending 8-7 [Memory Mapped]       

MsgValX          0x00000001    Message Valid X [Memory Mapped]         

MsgVal12        0x00000001    Message Valid 2-1 [Memory Mapped]         

MsgVal34        0x00000000    Message Valid 4-3 [Memory Mapped]         

MsgVal56        0x00000000    Message Valid 6-5 [Memory Mapped]         

MsgVal78        0x00000000    Message Valid 8-7 [Memory Mapped]         

IntPndMx12     0x00000000    IntPndMux 2-1 [Memory Mapped]         

IntPndMx34     0x00000000    IntPndMux 4-3 [Memory Mapped]         

IntPndMx56     0x00000000    IntPndMux 6-5 [Memory Mapped]         

IntPndMx78     0x00000000    IntPndMux 8-7 [Memory Mapped]         

If1Cmd 0x00870001    If1 Command Mask / Command Request Register [Memory Mapped]  

If1Msk  0xE00007FF    If1 Mask Register [Memory Mapped]           

If1Arb   0xE0000001    If1 Arbitation Register [Memory Mapped]         

If1MsgCtrl        0x00001008    If1 Message Control Register [Memory Mapped]    

If1DatA            0x00000000    If1 Data A Register [Memory Mapped]         

If1DatB            0x00000000    If1 Data B Register [Memory Mapped]         

If2Com 0x00170001    If2 Command Mask / Command Request Register [Memory Mapped]  

If2Msk  0xFFFFFFFF   If2 Mask Register [Memory Mapped]           

If2Arb   0x00000000    If2 Arbitation Register [Memory Mapped]         

If2MsgCtrl        0x00000000    If2 Message Control Register [Memory Mapped]    

If2DatA            0x00000000    If2 Data A Register [Memory Mapped]         

If2DatB            0x00000000    If2 Data B Register [Memory Mapped]         

If3Obs  0x00000000    If3 Observation Register [Memory Mapped]         

If3Msk  0xFFFFFFFF   If3 Mask Register [Memory Mapped]           

If3Arb   0x00000000    If3 Arbitation Register [Memory Mapped]         

If3MsgCtrl        0x00000000    If3 Message Control Register [Memory Mapped]    

If3DatA            0x00000000    If3 Data A Register [Memory Mapped]         

If3DatB            0x00000000    If3 Data B Register [Memory Mapped]         

If3Upd12          0x00000000    Update enable 2-1 Register [Memory Mapped]       

If3Upd34          0x00000000    Update enable 4-3 Register [Memory Mapped]       

If3Upd56          0x00000000    Update enable 6-5 Register [Memory Mapped]       

If3Upd78          0x00000000    Update enable 8-7 Register [Memory Mapped]       

IoCtrlTx            0x0004000E    TX IO Control Register [Memory Mapped]       

IoCtrlRx           0x00040009    RX IO Control Register [Memory Mapped]       

 

 

6、对比测试:

1)我们现在测试的两块板子都有如此问题,不能正常发送CAN。使用内部还回测试是正常的。

2)使用3137开发板,按照如上方式建立最简单的工程,测试是成功的。

  • 请问您的板子是TI的还是自己设计的呢?如果是自己的板子,芯片焊接是否有问题?
    是否有用示波器测can的发送引脚?
  • 板子是我们自己开发的。已经使用示波器监测了引脚的信号,没有有效的波形输出。

    在3137的开发板上对应的MCU引脚可以看到正确的波形。

  • Hi David,
    1. 在你的电路中,看你使用的CAN1。LS2135有3路CAN,建议测一下其他两路CAN,看是否同样没有波形输出?

    2. 检查电路中的CAN1_STATE是否能够按你的程序自主控制,或者直接将SN65HVDA541的STB/S引脚拉高,再重新测试。

    3. 能否上传你们测试到的CAN的波形?

    4. 切断收发器与TMS570的连接,测试TMS570侧CAN1TX,CAN1RX的波形输出。