参照了别的Hercules MCU的例子,写了一个demo,不起作用,不知道问题在哪!
/* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "sys_common.h"
/* USER CODE BEGIN (1) */
#include <mibspi.h>
#include <sys_dma.h>
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define D_SIZE 64
uint16 tx_data[D_SIZE] = {0};
uint16 rx_data[D_SIZE] = {0};
g_dmaCTRL g_dmaCTRL_tx;
g_dmaCTRL g_dmaCTRL_rx;
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
sint32 i;
for (i = 0; i < D_SIZE; i++)
{
tx_data[i] = i;
}
mibspiInit();
mibspiEnableLoopback(mibspiREG1, Analog_Lbk);
dmaEnable();
//mibspiSetData(mibspiREG1, 0, tx_data);
dmaReqAssign(DMA_CH0, 1u);
g_dmaCTRL_tx.SADD = (uint32)(&tx_data);
g_dmaCTRL_tx.DADD = (uint32)(&(mibspiRAM1->tx[0]));
g_dmaCTRL_tx.CHCTRL = DMA_CH0;
g_dmaCTRL_tx.FRCNT = 1u;
g_dmaCTRL_tx.ELCNT = D_SIZE;
g_dmaCTRL_tx.ELDOFFSET = 4u;
g_dmaCTRL_tx.ELSOFFSET = 0u;
g_dmaCTRL_tx.FRDOFFSET = 0u;
g_dmaCTRL_tx.FRSOFFSET = 0u;
g_dmaCTRL_tx.PORTASGN = 4u;
g_dmaCTRL_tx.RDSIZE = ACCESS_16_BIT;
g_dmaCTRL_tx.WRSIZE = ACCESS_16_BIT;
g_dmaCTRL_tx.TTYPE = FRAME_TRANSFER;
g_dmaCTRL_tx.ADDMODERD = ADDR_INC1;
g_dmaCTRL_tx.ADDMODEWR = ADDR_OFFSET;
g_dmaCTRL_tx.AUTOINIT = AUTOINIT_ON;
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRL_tx);
dmaSetChEnable(DMA_CH0, DMA_HW);
mibspiREG1->DMACTRL[0] |= (((1 << 4) | 0) << 16);
mibspiREG1->DMACTRL[0] |= 0x8000C000u;
mibspiREG1->DMACTRL[0] |= (0 << 8) |(0 << 24);
mibspiTransfer(mibspiREG1,0 );
while (!(mibspiIsTransferComplete(mibspiREG1,0))) {}
mibspiGetData(mibspiREG1, 0, rx_data);
while (true) {}
/* USER CODE END */
//return 0;
}