This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI官网提供的TMS570LS31x 原理图



TI官网提供的TMS570LS31x 原理图,有一下几个问题咨询:

1. 原理图中,个别电阻、电容value都写得NOP,代表什么意思?

2. POR_RESET和WARM_RESET,与JTAG的复位ARM_JTAG_RESET,三个引脚应如何连接?

如果使用TPS3802K33能否复位WARM_RESET,与ARM_JTAG_RESET连在一起,同时作用;POR_RESET能否只做上拉处理?

目前的接法,手动复位按钮无法通过TPS3802K33对cpu进行复位,RESET引脚输出的高电平一直是0.24V,按下按钮后是0V,cpu始终处于复位状态。不知道是什么原因。

3. 晶振部分能否如下图,XTAL接入CPU的OSCIN?是否必须像原理图中那样的接法?

如果下图接法可以,那么OSCOUT、KELVIN-GND、ECLK和EXTCLKIN,这四个引脚需要做什么处理?

谢谢!