This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0432 LaunchPad CAN通信异常

Other Parts Discussed in Thread: TMS570LS0432

我使用的开发板是 Hercules TMS570L4x LaunchPad;芯片型号是TMS570LS0432

 

1 完全按照HCG的帮助文件example_canCommunication.c例程配置相应寄存器;

(1)勾选Enable CAN1 driver、勾选Enable CAN1 driver、勾选EnableDCC driver;

(2)CAN1、CAN2都选择500Kbi波特率,勾选Enable Identifier Extension;

(3)Active CAN1 Message1 configuration,选择Tx功能;

(4)Active CAN2 Message1 cnofiguration,选择Rx功能;

2 由于Hercules TMS570L4x LaunchPad的CAN通信接口没有电平转化,

现分别给CAN1 和 CAN2 的pin脚外加了VP230模块(CAN1一个、CAN2一个),

即 CAN1 Tx、CAN1Rx接VP230模块1的 Tx、Rx;

CAN2 Tx、CAN2Rx接VP230模块2的 Tx、Rx;

VP230模块1的H、L与VP230模块2的H、L相连;

3 调试程序,程序一直停留在这里,下不去;
 while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1));

 

uint32 canIsRxMessageArrived(canBASE_t *node, uint32 messageBox)
{
uint32 flag;
uint32 regIndex = (messageBox - 1U) >> 5U;
uint32 bitIndex = 1U << ((messageBox - 1U) & 0x1FU);

/* USER CODE BEGIN (16) */
/* USER CODE END */

/** - Read Tx request register */
flag = node->NWDATx[regIndex] & bitIndex;///////////////////////flag 总是为0

/* USER CODE BEGIN (17) */
/* USER CODE END */

return flag;
}

我想咨询的问题是:
1 配驱动时一定要配置---------》勾选EnableDCC driver;为什么?
2 我的外接的模块的电路有问题么?

代码想要实现CAN1 Message1 发送数据,CAN2 Message2 接收回数据
main.c的代码

#include "sys_common.h"

/* USER CODE BEGIN (1) */
#include "system.h"
#include "can.h"
#include "esm.h"

#define  D_SIZE 9
uint8  tx_data[D_SIZE]  = {'H','E','R','C','U','L','E','S','\0'};
uint8  rx_data[D_SIZE] = {0};
uint32 error = 0;
uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize);
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */
   canInit(); /* can1 -> can2 */   
   /* transmit on can1 */    
   canTransmit(canREG1, canMESSAGE_BOX1, tx_data);     
   /*... wait until message receive on can2 */    
   while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1));
   canGetData(canREG2, canMESSAGE_BOX1, rx_data);  /* receive on can2  */    
   /* check received data patterns */    
   error = checkPackets(&tx_data[0],&rx_data[0],D_SIZE);    
   /* ... run forever */    
   while(1);

/* USER CODE END */

    return 0;
}


/* USER CODE BEGIN (4) */
uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize)
{   
uint32 err=0;   
uint32 cnt=psize;   
while(cnt--)   
{     
if((*src_packet++) != (*dst_packet++))     
{        
err++;           /*  data error  */     
}   
}   
return (err);
}

1385.can6.zip

 

  • 双时钟比较器(DCC)模块通过计算两个独立时钟源的脉冲(计数器0和计数器1)来确定可选择时钟源的精度。如果一个时钟超出了规范,就会产生一个错误信号。例如,DCC可以配置为使用CLK10M作为参考时钟(对于计数器0),VCLK作为“正在测试的时钟”(对于计数器1)。
    为了给CAN提供准确的时钟。