This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0714无法烧录,芯片一直自动运行的问题

自己做的一块板子,使用JTAG烧录时,单片机一直处于running状态,导致无法烧录。

用XDS100烧录时提示以下问题,有朋友遇到这个问题吗?

用劳特巴赫烧录时也提示类似异常(access timeout,processor running)。

CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: Trouble Removing Breakpoint with the Action "Remain Halted" at 0x8000128: (Error -1066 @ 0x8000128) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 7.0.188.0)
CortexR4: File Loader: Memory write failed: Timed out waiting for target to halt while executing wr_pll.alg
CortexR4: GEL: File: D:\02_Peoject\02_Software\workplace\570Error\Debug\570ERROR.out: Load failed.
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset

  • 下载工具没有问题 另一块板子XDS100和劳特巴赫都可以烧录的。

    关键应该是下面的提示

    CortexR4: Trouble Removing Breakpoint with the Action "Remain Halted" at 0x80004c0: (Error -1066 @ 0x80004C0) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 7.0.188.0)
    CortexR4: File Loader: Memory write failed: Timed out waiting for target to halt while executing erasew.alg
    CortexR4: GEL: File: D:\02_Peoject\02_Software\workplace\570Error\Debug\570ERROR.out: Load failed.

  • 可能芯片内的某固件搞丢了
    错误代码一样
    e2e.ti.com/.../2196967


    错误代码类似,第八节内容
    www.21ic.com/.../650476_4.htm

    你试试看看是不是类似这种问题导致的。