刚从C2000系列转到ARM570,驱动都配置得差不多了,我有以下疑问请大家帮我看看,
1.首先就是我在用DEMO板仿真的时候,我发现通过仿真器程序是直接烧进FLASH的,掉电程序不会丢失,不像C2000有RAM和FLASH两个CMD,可以选择烧入FLASH还是RAM,我的理解对吗?
2.C2000为了加快执行速度,会把FLASH中的一些函数拷贝到RAM中执行,使用#pragma CODE_SECTION(xxxxxx, "ramfuncs");就可以了,570有内置这样的预编译指令吗?怎么实现这个功能呢?