This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在接收CAN数据的时候,Message Identifier怎么理解?

Other Parts Discussed in Thread: HALCOGEN

你好!

我在调试通过TMS570 DCAN接收毫米波雷达ARS408的数据的时候遇到问题,怎么也收不到数据。

我是通过将示例程序里的example_canCommunication.c修改一下来进行调试的,就是不再向CAN1发送数据,直接从CAN2接收数据,CAN2接到毫米波雷达的CAN口。

现在只知道毫米波雷达的位速率是500k bits/s,这个例子本身也是配的500k bits/s。can.c中关于canReg2部分的设置代码如下:


    /** @b Initialize @b CAN2: */

    /** - Setup control register
    *     - Disable automatic wakeup on bus activity
    *     - Local power down mode disabled
    *     - Disable DMA request lines
    *     - Enable global Interrupt Line 0 and 1
    *     - Disable debug mode
    *     - Release from software reset
    *     - Enable/Disable parity or ECC
    *     - Enable/Disable auto bus on timer
    *     - Setup message completion before entering debug state
    *     - Setup normal operation mode
    *     - Request write access to the configuration registers
    *     - Setup automatic retransmission of messages
    *     - Disable error interrupts
    *     - Disable status interrupts
    *     - Enter initialization mode
    */
    canREG2->CTL = (uint32)0x00000000U
                 | (uint32)0x00000000U
                 | (uint32)((uint32)0x00000005U << 10U)
                 | 0x00020043U;

    /** - Clear all pending error flags and reset current status */
    canREG2->ES |= 0xFFFFFFFFU;

    /** - Assign interrupt level for messages */
    canREG2->INTMUXx[0U] = (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U;

    canREG2->INTMUXx[1U] = (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U
                         | (uint32)0x00000000U;


    /** - Setup auto bus on timer period */
    canREG2->ABOTR = (uint32)0U;


    /** - Initialize message 1
    *     - Wait until IF1 is ready for use
    *     - Set message mask
    *     - Set message control word
    *     - Set message arbitration
    *     - Set IF1 control byte
    *     - Set IF1 message number
    */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
    while ((canREG2->IF1STAT & 0x80U) ==0x80U)
    {
    } /* Wait */


    //canREG2->IF1MSK  = 0xC0000000U | (uint32)((uint32)((uint32)0x000007FFU & (uint32)0x1FFFFFFFU) << (uint32)0U);
    canREG2->IF1MSK  = 0x00000000U;
    //canREG2->IF1ARB  = (uint32)0x80000000U | (uint32)0x40000000U | (uint32)0x00000000U | (uint32)((uint32)((uint32)1U & (uint32)0x1FFFFFFFU) << (uint32)0U);
    canREG2->IF1ARB  = (uint32)0x80000000U | (uint32)0x40000000U | (uint32)0x00000000U;
    //canREG2->IF1MCTL = 0x00001080U | (uint32)0x00000000U | (uint32)0x00000000U | (uint32)8U;
    canREG2->IF1MCTL = 0x00000080U | (uint32)0x00000000U | (uint32)0x00000000U | (uint32)8U;
    canREG2->IF1CMD  = (uint8) 0xF8U;
    canREG2->IF1NO   = 1U;

    /** - Setup IF1 for data transmission
    *     - Wait until IF1 is ready for use
    *     - Set IF1 control byte
    */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
    while ((canREG2->IF1STAT & 0x80U) ==0x80U)
    {
    } /* Wait */
    canREG2->IF1CMD  = 0x87U;

    /** - Setup IF2 for reading data
    *     - Wait until IF1 is ready for use
    *     - Set IF1 control byte
    */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
    while ((canREG2->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */
    canREG2->IF2CMD = 0x17U;

    /** - Setup bit timing
    *     - Setup baud rate prescaler extension
    *     - Setup TSeg2
    *     - Setup TSeg1
    *     - Setup sample jump width
    *     - Setup baud rate prescaler
    */
    canREG2->BTR = (uint32)((uint32)0U << 16U) |
                   (uint32)((uint32)(3U - 1U) << 12U) |
                   (uint32)((uint32)((5U + 3U) - 1U) << 8U) |
                   (uint32)((uint32)(3U - 1U) << 6U) |
                   (uint32)14U;        


   /** - CAN2 Port output values */
    canREG2->TIOC =  (uint32)((uint32)1U  << 18U )
                   | (uint32)((uint32)0U  << 17U )
                   | (uint32)((uint32)0U  << 16U )  
                   | (uint32)((uint32)1U  << 3U )  
                   | (uint32)((uint32)1U  << 2U )    
                   | (uint32)((uint32)1U << 1U );
                   
    canREG2->RIOC =  (uint32)((uint32)1U  << 18U )    
                   | (uint32)((uint32)0U  << 17U )  
                   | (uint32)((uint32)0U  << 16U )   
                   | (uint32)((uint32)1U  << 3U )  
                   | (uint32)((uint32)0U  << 2U )
                   | (uint32)((uint32)0U <<1U );   

    /** - Leave configuration and initialization mode  */
    canREG2->CTL &= ~(uint32)(0x00000041U);

我的问题是 canREG2->IF1ARB 中的 Xtd 和 ID[28:0] 貌似很重要,因为我从DCAN1发送数据到DCAN2,如果更改了接收方的 Xtd 和 Message Identifier,会接收不到数据,Xtd应该是表示帧格式是 Standard Frame or Extended Frame, 那 Message Identifier 怎么理解昵?

另外,只知道毫米波雷达的位速率为500k的情况下能正确接收到数据吗?(不知道 Xtd 和 Message Identifier),还有我想不用 acceptance filtering,我的代码里的改动正确吗? (将canREG2->IF1MSK 设为全0, 将 canREG2->IF1MCTL 中的 UMask 设为0)