Other Parts Discussed in Thread: LAUNCHXL-TMS57004
我在电源管理方面是个新手,近期想购买你们的一些电子元件,因为我想针对你们官网的TMS570BMS进行研究和学习。我想在你们MS570BMS的基础上设计符合我需要的电源管理,因为我需要的是为我们实验室的一个小型的电动小汽车进行供电和实现电源管理,所需要的电池电压为48 V容量为20AH,一般的锂离子电池的工作电压为3.7v容量为2000mah,因此我需要选择额13串10并的连接方式组成电池组供电。因为根据我现在的了解,你们公司针对电源管理的元器件也都是针对汽车级的,然而汽车中应用的电池组中的电池也是既有并联也有串联的连接方式,所以我想知道是针对TMS570BMS的设计方案是不是也可以实现对高电压、大容量的串并联电池组进行电源管理的?
1、因为针对TMS570BMS的均衡设计,如果采用你们的EM1402EVM均衡评估板,我想知道的是你们这个板子均衡的依据是什么?电池的电压吗?如果均衡的依据是电池的电压均衡,那按原理分析的话按照我需要的48V20AH的需求的话,是13串10并,也是可以实现的吧!因为虽然我需要的电池组中的电池连接方式是既有串联也有并联的,并不是你们官网上样品那样只是16节电池单体串联监测均衡。我的电池组虽然电池有并联的,但是并联起来的电池电压是一致的,并联只是增加电池组的容量,如果均衡的标准是电压,我的设计也是可以实现的对吗?只需要监测13节串联起来的电池即可对吗?
2、针对LAUNCHXL-TMS57004评估板是否有示例代码?
希望专业人士可以帮我解决下这些问题,谢谢!