This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好!
此次使用的芯片是TMS570LS0232,使用HAL Code Generator 配置好后,进行调试。
程序如下:
static int WatValu;
int main(void)
{
while(1)
{
uint32 i;
if(WatValu)
WatValu = 0;
else WatValu = 1;
for(i=0;i<10000;i++);
}
}
运行后变量显示为BAD0,内存显示上发现各个地址上存放的数据均是BAD0;
在程序中加入断点后暂停时,观测值与内存地址上的值显示正常。
在此之前用过TMS570ls1114和1224的芯片,ram的值在监控界面的示数均可实时更新,出现过Flash中的值为BAD0的情况,通过屏蔽sys_startup.c文件中_coreEnableFlashEcc_()函数即可恢复正常。但此次TMS570LS0232的测试中,_coreEnableFlashEcc_(void);_coreEnableRamEcc_(void);均被屏蔽,但现象不变。
请问各位,1.TMS570系列显示BAD0的原因是什么? 如何使能禁能此项功能?